PLInterface.InterfaceAppletStatusEnum Class#
Applies to: CoaXPress
Visibility: Beginner
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLInterface.InterfaceAppletStatusEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLInterface.InterfaceAppletStatusEnum | Initializes a new instance of the PLInterface.InterfaceAppletStatusEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Acq_DualCXP12Area | The status of the Acq_DualCXP12Area applet is returned. Applies to: CoaXPress | |
Acq_DualCXP12Line | Applies to: CoaXPress | |
Acq_QuadCXP12Area | The status of the Acq_QuadCXP12Area applet is returned. Applies to: CoaXPress | |
Acq_QuadCXP12Line | Applies to: CoaXPress | |
Acq_SingleCXP12Area | The status of the Acq_SingleCXP12Area applet is returned. Applies to: CoaXPress | |
Acq_SingleCXP12Line | Applies to: CoaXPress | |
Acq_TripleCXP12Area | The status of the Acq_TripleCXP12Area applet is returned. Applies to: CoaXPress | |
Acq_TripleCXP12Line | Applies to: CoaXPress | |
FrameGrabberTest | Applies to: CoaXPress | |
Loading | The status of the applet is Loading. Applies to: CoaXPress | |
名前 | The full name of InterfaceAppletStatus (Overrides ParameterListEnum.Name.) | |
NotLoaded | The status of the applet is NotLoaded. Applies to: CoaXPress |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of InterfaceAppletStatus (Overrides Object.ToString()()()().) |
PLInterface.InterfaceAppletStatusEnum.ToString Method#
The full name of InterfaceAppletStatus
Return Value#
Type: String
Returns the full name of InterfaceAppletStatus
PLInterface.InterfaceAppletStatusEnum Constructor#
Initializes a new instance of the PLInterface.InterfaceAppletStatusEnum class
PLInterface.InterfaceAppletStatusEnum.Acq_DualCXP12Area Property#
The status of the Acq_DualCXP12Area applet is returned.
Applies to: CoaXPress
PLInterface.InterfaceAppletStatusEnum.Acq_DualCXP12Line Property#
Applies to: CoaXPress
PLInterface.InterfaceAppletStatusEnum.Acq_QuadCXP12Area Property#
The status of the Acq_QuadCXP12Area applet is returned.
Applies to: CoaXPress
PLInterface.InterfaceAppletStatusEnum.Acq_QuadCXP12Line Property#
Applies to: CoaXPress
PLInterface.InterfaceAppletStatusEnum.Acq_SingleCXP12Area Property#
The status of the Acq_SingleCXP12Area applet is returned.
Applies to: CoaXPress
PLInterface.InterfaceAppletStatusEnum.Acq_SingleCXP12Line Property#
Applies to: CoaXPress
PLInterface.InterfaceAppletStatusEnum.Acq_TripleCXP12Area Property#
The status of the Acq_TripleCXP12Area applet is returned.
Applies to: CoaXPress
PLInterface.InterfaceAppletStatusEnum.Acq_TripleCXP12Line Property#
Applies to: CoaXPress
PLInterface.InterfaceAppletStatusEnum.FrameGrabberTest Property#
Applies to: CoaXPress
PLInterface.InterfaceAppletStatusEnum.Loading Property#
The status of the applet is Loading.
Applies to: CoaXPress
PLInterface.InterfaceAppletStatusEnum.Name Property#
The full name of InterfaceAppletStatus
PLInterface.InterfaceAppletStatusEnum.NotLoaded Property#
The status of the applet is NotLoaded.
Applies to: CoaXPress