PLCamera.BslFlatFieldCorrectionModeEnum Class#
Applies to: boost_V_CoaXPress
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslFlatFieldCorrectionModeEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.BslFlatFieldCorrectionModeEnum | Initializes a new instance of the PLCamera.BslFlatFieldCorrectionModeEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
DSNUOnly | Only Dark Signal Non-Uniformity (DSNU) correction is performed. Applies to: boost_V_CoaXPress | |
名前 | The full name of BslFlatFieldCorrectionMode (Overrides ParameterListEnum.Name.) | |
Off | Flat-field correction is disabled. Applies to: boost_V_CoaXPress | |
その | Flat-field correction is enabled. Dark signal non-uniformities (DSNU) and photo response non-uniformities (PRNU) will be corrected. Applies to: boost_V_CoaXPress |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of BslFlatFieldCorrectionMode (Overrides Object.ToString()()()().) |
PLCamera.BslFlatFieldCorrectionModeEnum.ToString Method#
The full name of BslFlatFieldCorrectionMode
Return Value#
Type: String
Returns the full name of BslFlatFieldCorrectionMode
PLCamera.BslFlatFieldCorrectionModeEnum Constructor#
Initializes a new instance of the PLCamera.BslFlatFieldCorrectionModeEnum class
PLCamera.BslFlatFieldCorrectionModeEnum.DSNUOnly Property#
Only Dark Signal Non-Uniformity (DSNU) correction is performed.
Applies to: boost_V_CoaXPress
PLCamera.BslFlatFieldCorrectionModeEnum.Name Property#
The full name of BslFlatFieldCorrectionMode
PLCamera.BslFlatFieldCorrectionModeEnum.Off Property#
Flat-field correction is disabled.
Applies to: boost_V_CoaXPress
PLCamera.BslFlatFieldCorrectionModeEnum.On Property#
Flat-field correction is enabled. Dark signal non-uniformities (DSNU) and photo response non-uniformities (PRNU) will be corrected.
Applies to: boost_V_CoaXPress