PLCamera.FrequencyConverterSignalAlignmentEnum Class#
Applies to: CameraLink and GigE
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.FrequencyConverterSignalAlignmentEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.FrequencyConverterSignalAlignmentEnum | Initializes a new instance of the PLCamera.FrequencyConverterSignalAlignmentEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
FallingEdge | For the falling edge of each signal received from the pre-divider sub-module, a phase-locked falling edge of a signal generated by the multiplier sub-module is provided. Applies to: CameraLink and GigE | |
名前 | The full name of FrequencyConverterSignalAlignment (Overrides ParameterListEnum.Name.) | |
RisingEdge | For the rising edge of each signal received from the pre-divider sub-module, a phase-locked rising edge of a signal generated by the multiplier sub-module is provided. Applies to: CameraLink and GigE |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of FrequencyConverterSignalAlignment (Overrides Object.ToString()()()().) |
PLCamera.FrequencyConverterSignalAlignmentEnum.ToString Method#
The full name of FrequencyConverterSignalAlignment
Return Value#
Type: String
Returns the full name of FrequencyConverterSignalAlignment
PLCamera.FrequencyConverterSignalAlignmentEnum Constructor#
Initializes a new instance of the PLCamera.FrequencyConverterSignalAlignmentEnum class
PLCamera.FrequencyConverterSignalAlignmentEnum.FallingEdge Property#
For the falling edge of each signal received from the pre-divider sub-module, a phase-locked falling edge of a signal generated by the multiplier sub-module is provided.
Applies to: CameraLink and GigE
PLCamera.FrequencyConverterSignalAlignmentEnum.Name Property#
The full name of FrequencyConverterSignalAlignment
PLCamera.FrequencyConverterSignalAlignmentEnum.RisingEdge Property#
For the rising edge of each signal received from the pre-divider sub-module, a phase-locked rising edge of a signal generated by the multiplier sub-module is provided.
Applies to: CameraLink and GigE