PLCamera.AutoFunctionProfileEnum Class#
Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and pulse USB
Visibility: Beginner
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.AutoFunctionProfileEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.AutoFunctionProfileEnum | Initializes a new instance of the PLCamera.AutoFunctionProfileEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
AntiFlicker50Hz | Gain and exposure time are optimized to reduce flickering in an environment where the lighting flickers at a 50-Hz rate (e.g., Europe). Applies to: dart USB and pulse USB | |
AntiFlicker60Hz | Gain and exposure time are optimized to reduce flickering in an environment where the lighting flickers at a 60-Hz rate (e.g., North America). Applies to: dart USB and pulse USB | |
ExposureMinimum | Exposure time is kept as low as possible during automatic adjustments. Applies to: CameraLink and GigE | |
ExposureMinimumQuick | Exposure time is kept as low as possible and is adjusted quickly. Applies to: GigE | |
GainMinimum | Gain is kept as low as possible during automatic adjustments. Applies to: CameraLink and GigE | |
GainMinimumQuick | Gain time is kept as low as possible and is adjusted quickly. Applies to: GigE | |
MinimizeExposureTime | Exposure time is kept as low as possible during automatic adjustments. Applies to: ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and pulse USB | |
MinimizeExposureTimeQuick | Exposure time is kept as low as possible and is adjusted quickly when there are extreme or rapid changes in brightness. Applies to: ace USB | |
MinimizeGain | Gain is kept as low as possible during automatic adjustments. Applies to: ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and pulse USB | |
MinimizeGainQuick | Gain is kept as low as possible and is adjusted quickly when there are extreme or rapid changes in brightness. Applies to: ace USB | |
名前 | The full name of AutoFunctionProfile (Overrides ParameterListEnum.Name.) | |
Smart | Gain is kept as low as possible and the frame rate is kept as high as possible during automatic adjustments. Applies to: dart USB and pulse USB |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of AutoFunctionProfile (Overrides Object.ToString()()()().) |
PLCamera.AutoFunctionProfileEnum.ToString Method#
The full name of AutoFunctionProfile
Return Value#
Type: String
Returns the full name of AutoFunctionProfile
PLCamera.AutoFunctionProfileEnum Constructor#
Initializes a new instance of the PLCamera.AutoFunctionProfileEnum class
PLCamera.AutoFunctionProfileEnum.AntiFlicker50Hz Property#
Gain and exposure time are optimized to reduce flickering in an environment where the lighting flickers at a 50-Hz rate (e.g., Europe).
Applies to: dart USB and pulse USB
PLCamera.AutoFunctionProfileEnum.AntiFlicker60Hz Property#
Gain and exposure time are optimized to reduce flickering in an environment where the lighting flickers at a 60-Hz rate (e.g., North America).
Applies to: dart USB and pulse USB
PLCamera.AutoFunctionProfileEnum.ExposureMinimum Property#
Exposure time is kept as low as possible during automatic adjustments.
Applies to: CameraLink and GigE
PLCamera.AutoFunctionProfileEnum.ExposureMinimumQuick Property#
Exposure time is kept as low as possible and is adjusted quickly.
Applies to: GigE
PLCamera.AutoFunctionProfileEnum.GainMinimum Property#
Gain is kept as low as possible during automatic adjustments.
Applies to: CameraLink and GigE
PLCamera.AutoFunctionProfileEnum.GainMinimumQuick Property#
Gain time is kept as low as possible and is adjusted quickly.
Applies to: GigE
PLCamera.AutoFunctionProfileEnum.MinimizeExposureTime Property#
Exposure time is kept as low as possible during automatic adjustments.
Applies to: ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and pulse USB
PLCamera.AutoFunctionProfileEnum.MinimizeExposureTimeQuick Property#
Exposure time is kept as low as possible and is adjusted quickly when there are extreme or rapid changes in brightness.
Applies to: ace USB
PLCamera.AutoFunctionProfileEnum.MinimizeGain Property#
Gain is kept as low as possible during automatic adjustments.
Applies to: ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress, dart 2 USB, dart USB and pulse USB
PLCamera.AutoFunctionProfileEnum.MinimizeGainQuick Property#
Gain is kept as low as possible and is adjusted quickly when there are extreme or rapid changes in brightness.
Applies to: ace USB
PLCamera.AutoFunctionProfileEnum.Name Property#
The full name of AutoFunctionProfile
PLCamera.AutoFunctionProfileEnum.Smart Property#
Gain is kept as low as possible and the frame rate is kept as high as possible during automatic adjustments.
Applies to: dart USB and pulse USB