PLCamera.GevInterfaceSelectorEnum Class#
Applies to: GigE
Visibility: Guru
Selecting Parameters: GevCurrentDefaultGateway, GevCurrentIPAddress, GevCurrentIPConfiguration, GevCurrentSubnetMask, GevLinkCrossover, GevLinkFullDuplex, GevLinkMaster, GevLinkSpeed, GevMACAddress, GevPersistentDefaultGateway, GevPersistentIPAddress, GevPersistentSubnetMask, GevSupportedIPConfigurationDHCP, GevSupportedIPConfigurationLLA, GevSupportedIPConfigurationPersistentIP, GevSupportedOptionalLegacy16BitBlockID
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.GevInterfaceSelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.GevInterfaceSelectorEnum | Initializes a new instance of the PLCamera.GevInterfaceSelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
名前 | The full name of GevInterfaceSelector (Overrides ParameterListEnum.Name.) | |
NetworkInterface0 | Network interface 0 can be configured. Applies to: GigE |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of GevInterfaceSelector (Overrides Object.ToString()()()().) |
PLCamera.GevInterfaceSelectorEnum.ToString Method#
The full name of GevInterfaceSelector
Return Value#
Type: String
Returns the full name of GevInterfaceSelector
PLCamera.GevInterfaceSelectorEnum Constructor#
Initializes a new instance of the PLCamera.GevInterfaceSelectorEnum class
PLCamera.GevInterfaceSelectorEnum.Name Property#
The full name of GevInterfaceSelector
PLCamera.GevInterfaceSelectorEnum.NetworkInterface0 Property#
Network interface 0 can be configured.
Applies to: GigE