PLCamera.CounterEventSourceEnum Class#
Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB
Visibility: Beginner
Selected by: CounterSelector
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.CounterEventSourceEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.CounterEventSourceEnum | Initializes a new instance of the PLCamera.CounterEventSourceEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
AcquisitionActive | The selected counter counts the number of Acquisition Active signals. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
AcquisitionEnd | Counts the number of Acquisition End. Applies to: CameraLink and GigE | |
AcquisitionStart | Counts the number of Acquisition Start. Applies to: CameraLink and GigE | |
AcquisitionTrigger | Counts the number of Acquisition Trigger. Applies to: CameraLink and GigE | |
Action1 | The selected counter counts the number of action commands received for action signal 1. Applies to: ace 2 GigE | |
Action2 | The selected counter counts the number of action commands received for action signal 2. Applies to: ace 2 GigE | |
Counter1Active | The selected counter counts the number of Counter 1 Active signals. By default, a Counter 1 Active signal is generated whenever counter 1 is started. You can change this behavior using the Counter Event Activation parameter. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Counter1End | The selected counter counts the number of Counter 1 End signals. A Counter 1 End signal is generated whenever counter 1 is stopped, reset, or when it has reached its maximum value. Applies to: ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB | |
Counter1Start | The selected counter counts the number of Counter 1 Start signals. A Counter 1 Start signal is generated whenever counter 1 is started. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Counter2Active | The selected counter counts the number of Counter 2 Active signals. By default, a Counter 2 Active signal is generated whenever counter 2 is started. You can change this behavior using the Counter Event Activation parameter. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Counter2End | The selected counter counts the number of Counter 2 End signals. A Counter 2 End signal is generated whenever counter 2 is stopped, reset, or when it has reached its maximum value. Applies to: ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB | |
Counter2Start | The selected counter counts the number of Counter 2 Start signals. A Counter 2 Start signal is generated whenever counter 2 is started. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Counter3End | The selected counter counts the number of counter 3 end events. Applies to: ace USB | |
CxpTrigger0 | The selected counter counts the number of CXP Trigger 0 signals. Applies to: boost CoaXPress | |
CxpTrigger1 | The selected counter counts the number of CXP Trigger 1 signals. Applies to: boost CoaXPress | |
ExposureActive | The selected counter counts the number of Exposure Active signals. By default, an Exposure Active signal is generated whenever exposure is started. You can change this behavior using the Counter Event Activation parameter. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
ExposureEnd | Counts the number of Exposure End. Applies to: CameraLink and GigE | |
ExposureStart | The selected counter counts the number of Exposure Start signals. Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
ExposureTriggerWait | The selected counter counts the number of Exposure Trigger Wait signals. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
FrameBurstActive | The selected counter counts the number of Frame Burst Active signals. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
FrameBurstTriggerWait | The selected counter counts the number of Frame Burst Trigger Wait signals. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
FrameEnd | Counts the number of Frame End. Applies to: CameraLink and GigE | |
FrameStart | The selected counter counts the number of Frame Start events. Applies to: CameraLink, GigE and ace USB | |
FrameTrigger | The selected counter counts the number of Frame Trigger events. Applies to: CameraLink, GigE and ace USB | |
FrameTriggerWait | The selected counter counts the number of Frame Trigger Wait signals. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Line1 | The selected counter counts the number of Line 1 signals. A Line 1 signal is generated whenever the input or output signal on Line 1 changes as specified by the Counter Event Activation parameter. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Line2 | The selected counter counts the number of Line 2 signals. A Line 2 signal is generated whenever the input or output signal on Line 2 changes as specified by the Counter Event Activation parameter. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Line3 | The selected counter counts the number of Line 3 signals. A Line 3 signal is generated whenever the input or output signal on Line 3 changes as specified by the Counter Event Activation parameter. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Line4 | The selected counter counts the number of Line 4 signals. A Line 4 signal is generated whenever the input or output signal on Line 4 changes as specified by the Counter Event Activation parameter. Applies to: dart 2 USB | |
LineEnd | Counts the number of Line End. Applies to: CameraLink and GigE | |
LineStart | Counts the number of Line Start. Applies to: CameraLink and GigE | |
LineTrigger | The selected counter counts the number of Line Trigger events. Applies to: CameraLink and GigE | |
名前 | The full name of CounterEventSource (Overrides ParameterListEnum.Name.) | |
Off | The selected counter is disabled. Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
PeriodicSignal1 | The selected counter counts the number of Periodic Signal 1 signals. Applies to: ace 2 GigE | |
SoftwareSignal1 | The selected counter counts the number of Software Signal 1 signals. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
SoftwareSignal2 | The selected counter counts the number of Software Signal 2 signals. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
SoftwareSignal3 | The selected counter counts the number of Software Signal 3 signals. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Timer1Active | The selected counter counts the number of Timer 1 Active signals. By default, a Timer 1 Active signal is generated whenever timer 1 is started. You can change this behavior using the Counter Event Activation parameter. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Timer1End | The selected counter counts the number of Timer 1 End signals. A Timer 1 End signal is generated whenever timer 1 has elapsed. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Timer2Active | The selected counter counts the number of Timer 2 Active signals. By default, a Timer 2 Active signal is generated whenever timer 2 is started. You can change this behavior using the Counter Event Activation parameter. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Timer2End | The selected counter counts the number of Timer 2 End signals. A Timer 2 End signal is generated whenever timer 2 has elapsed. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of CounterEventSource (Overrides Object.ToString()()()().) |
PLCamera.CounterEventSourceEnum.ToString Method#
The full name of CounterEventSource
Return Value#
Type: String
Returns the full name of CounterEventSource
PLCamera.CounterEventSourceEnum Constructor#
Initializes a new instance of the PLCamera.CounterEventSourceEnum class
PLCamera.CounterEventSourceEnum.AcquisitionActive Property#
The selected counter counts the number of Acquisition Active signals.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.CounterEventSourceEnum.AcquisitionEnd Property#
Counts the number of Acquisition End.
Applies to: CameraLink and GigE
PLCamera.CounterEventSourceEnum.AcquisitionStart Property#
Counts the number of Acquisition Start.
Applies to: CameraLink and GigE
PLCamera.CounterEventSourceEnum.AcquisitionTrigger Property#
Counts the number of Acquisition Trigger.
Applies to: CameraLink and GigE
PLCamera.CounterEventSourceEnum.Action1 Property#
The selected counter counts the number of action commands received for action signal 1.
Applies to: ace 2 GigE
PLCamera.CounterEventSourceEnum.Action2 Property#
The selected counter counts the number of action commands received for action signal 2.
Applies to: ace 2 GigE
PLCamera.CounterEventSourceEnum.Counter1Active Property#
The selected counter counts the number of Counter 1 Active signals. By default, a Counter 1 Active signal is generated whenever counter 1 is started. You can change this behavior using the Counter Event Activation parameter.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.CounterEventSourceEnum.Counter1End Property#
The selected counter counts the number of Counter 1 End signals. A Counter 1 End signal is generated whenever counter 1 is stopped, reset, or when it has reached its maximum value.
Applies to: ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB
PLCamera.CounterEventSourceEnum.Counter1Start Property#
The selected counter counts the number of Counter 1 Start signals. A Counter 1 Start signal is generated whenever counter 1 is started.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.CounterEventSourceEnum.Counter2Active Property#
The selected counter counts the number of Counter 2 Active signals. By default, a Counter 2 Active signal is generated whenever counter 2 is started. You can change this behavior using the Counter Event Activation parameter.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.CounterEventSourceEnum.Counter2End Property#
The selected counter counts the number of Counter 2 End signals. A Counter 2 End signal is generated whenever counter 2 is stopped, reset, or when it has reached its maximum value.
Applies to: ace 2 GigE, ace 2 USB, ace USB, boost CoaXPress and dart 2 USB
PLCamera.CounterEventSourceEnum.Counter2Start Property#
The selected counter counts the number of Counter 2 Start signals. A Counter 2 Start signal is generated whenever counter 2 is started.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.CounterEventSourceEnum.Counter3End Property#
The selected counter counts the number of counter 3 end events.
Applies to: ace USB
PLCamera.CounterEventSourceEnum.CxpTrigger0 Property#
The selected counter counts the number of CXP Trigger 0 signals.
Applies to: boost CoaXPress
PLCamera.CounterEventSourceEnum.CxpTrigger1 Property#
The selected counter counts the number of CXP Trigger 1 signals.
Applies to: boost CoaXPress
PLCamera.CounterEventSourceEnum.ExposureActive Property#
The selected counter counts the number of Exposure Active signals. By default, an Exposure Active signal is generated whenever exposure is started. You can change this behavior using the Counter Event Activation parameter.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.CounterEventSourceEnum.ExposureEnd Property#
Counts the number of Exposure End.
Applies to: CameraLink and GigE
PLCamera.CounterEventSourceEnum.ExposureStart Property#
The selected counter counts the number of Exposure Start signals.
Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.CounterEventSourceEnum.ExposureTriggerWait Property#
The selected counter counts the number of Exposure Trigger Wait signals.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.CounterEventSourceEnum.FrameBurstActive Property#
The selected counter counts the number of Frame Burst Active signals.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.CounterEventSourceEnum.FrameBurstTriggerWait Property#
The selected counter counts the number of Frame Burst Trigger Wait signals.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.CounterEventSourceEnum.FrameEnd Property#
Counts the number of Frame End.
Applies to: CameraLink and GigE
PLCamera.CounterEventSourceEnum.FrameStart Property#
The selected counter counts the number of Frame Start events.
Applies to: CameraLink, GigE and ace USB
PLCamera.CounterEventSourceEnum.FrameTrigger Property#
The selected counter counts the number of Frame Trigger events.
Applies to: CameraLink, GigE and ace USB
PLCamera.CounterEventSourceEnum.FrameTriggerWait Property#
The selected counter counts the number of Frame Trigger Wait signals.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.CounterEventSourceEnum.Line1 Property#
The selected counter counts the number of Line 1 signals. A Line 1 signal is generated whenever the input or output signal on Line 1 changes as specified by the Counter Event Activation parameter.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.CounterEventSourceEnum.Line2 Property#
The selected counter counts the number of Line 2 signals. A Line 2 signal is generated whenever the input or output signal on Line 2 changes as specified by the Counter Event Activation parameter.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.CounterEventSourceEnum.Line3 Property#
The selected counter counts the number of Line 3 signals. A Line 3 signal is generated whenever the input or output signal on Line 3 changes as specified by the Counter Event Activation parameter.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.CounterEventSourceEnum.Line4 Property#
The selected counter counts the number of Line 4 signals. A Line 4 signal is generated whenever the input or output signal on Line 4 changes as specified by the Counter Event Activation parameter.
Applies to: dart 2 USB
PLCamera.CounterEventSourceEnum.LineEnd Property#
Counts the number of Line End.
Applies to: CameraLink and GigE
PLCamera.CounterEventSourceEnum.LineStart Property#
Counts the number of Line Start.
Applies to: CameraLink and GigE
PLCamera.CounterEventSourceEnum.LineTrigger Property#
The selected counter counts the number of Line Trigger events.
Applies to: CameraLink and GigE
PLCamera.CounterEventSourceEnum.Name Property#
The full name of CounterEventSource
PLCamera.CounterEventSourceEnum.Off Property#
The selected counter is disabled.
Applies to: CameraLink, GigE, ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.CounterEventSourceEnum.PeriodicSignal1 Property#
The selected counter counts the number of Periodic Signal 1 signals.
Applies to: ace 2 GigE
PLCamera.CounterEventSourceEnum.SoftwareSignal1 Property#
The selected counter counts the number of Software Signal 1 signals.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.CounterEventSourceEnum.SoftwareSignal2 Property#
The selected counter counts the number of Software Signal 2 signals.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.CounterEventSourceEnum.SoftwareSignal3 Property#
The selected counter counts the number of Software Signal 3 signals.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.CounterEventSourceEnum.Timer1Active Property#
The selected counter counts the number of Timer 1 Active signals. By default, a Timer 1 Active signal is generated whenever timer 1 is started. You can change this behavior using the Counter Event Activation parameter.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.CounterEventSourceEnum.Timer1End Property#
The selected counter counts the number of Timer 1 End signals. A Timer 1 End signal is generated whenever timer 1 has elapsed.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.CounterEventSourceEnum.Timer2Active Property#
The selected counter counts the number of Timer 2 Active signals. By default, a Timer 2 Active signal is generated whenever timer 2 is started. You can change this behavior using the Counter Event Activation parameter.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.CounterEventSourceEnum.Timer2End Property#
The selected counter counts the number of Timer 2 End signals. A Timer 2 End signal is generated whenever timer 2 has elapsed.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB