PLCamera.BslDualROIRowSelectorEnum Class#
Applies to: boost_V_CoaXPress
Visibility: Expert
Selecting Parameters: BslDualROIRowOffset, BslDualROIRowSize
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslDualROIRowSelectorEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.BslDualROIRowSelectorEnum | Initializes a new instance of the PLCamera.BslDualROIRowSelectorEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
名前 | The full name of BslDualROIRowSelector (Overrides ParameterListEnum.Name.) | |
Row1 | Row 1 can be configured. Applies to: boost_V_CoaXPress | |
Row2 | Row 2 can be configured. Applies to: boost_V_CoaXPress |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of BslDualROIRowSelector (Overrides Object.ToString()()()().) |
PLCamera.BslDualROIRowSelectorEnum.ToString Method#
The full name of BslDualROIRowSelector
Return Value#
Type: String
Returns the full name of BslDualROIRowSelector
PLCamera.BslDualROIRowSelectorEnum Constructor#
Initializes a new instance of the PLCamera.BslDualROIRowSelectorEnum class
PLCamera.BslDualROIRowSelectorEnum.Name Property#
The full name of BslDualROIRowSelector
PLCamera.BslDualROIRowSelectorEnum.Row1 Property#
Row 1 can be configured.
Applies to: boost_V_CoaXPress
PLCamera.BslDualROIRowSelectorEnum.Row2 Property#
Row 2 can be configured.
Applies to: boost_V_CoaXPress