ICommandParameter Interface#
Syntax#
C#
VB
The ICommandParameter type exposes the following members.
プロパティ#
名前 | 説明 | |
---|---|---|
Advanced | The advanced parameter settings, if available. (Inherited from IParameter.) | |
FullName | The full name of the parameter including path information. (Inherited from IParameter.) | |
IsEmpty | Indicates if the parameter is empty. If true, the parameter is invalid or does not exist. If a requested parameter does not exist in a parameter collection, an empty parameter object will be returned to simplify handling. An empty parameter is never readable or writable. (Inherited from IParameter.) | |
IsReadable | Indicates if the parameter is readable. (Inherited from IParameter.) | |
IsWritable | Indicates if the parameter is writable. (Inherited from IParameter.) | |
名前 | The name of the parameter without path information. (Inherited from IParameter.) |
方法#
名前 | 説明 | |
---|---|---|
Execute | Executes the command and returns immediately. | |
IsExecuting | Indicates if the command is currently executing. | |
ParseAndSetValue | Parses the value as string and sets the value. (Inherited from IParameter.) | |
ToString | The parameter value as a string. (Inherited from IParameter.) |
Events#
名前 | 説明 | |
---|---|---|
ParameterChanged | This event fires after any of the parameter properties (value, readability, writability, or advanced parameter settings) have changed. (Inherited from IParameter.) | |
ParameterValueChanged | This event fires after the parameter value has changed. (Inherited from IParameter.) |
Extension Methods#
名前 | 説明 | |
---|---|---|
TryExecute | Executes the command and returns immediately if the parameter is writable. (Defined by ICommandParameterExtensions.) |
ICommandParameter.Execute Method#
Executes the command and returns immediately.
Syntax#
C#
VB
Remarks#
Preconditions:
- The parameter must be writable.
Error Safety: Can throw exceptions if the parameter is not writable or if accessing the camera failed.
ICommandParameter.IsExecuting Method#
Indicates if the command is currently executing.
Syntax#
C#
VB
Return Value#
Type: Boolean
Returns true if the command is currently executing, otherwise false.
Remarks#
Thread Safety: This method is synchronized with the source of the parameter collection, if any.
Error Safety: Can throw exceptions if accessing the camera failed.