PLCamera.BslPeriodicSignalSourceEnum Class#
Applies to: ace 2 GigE
Visibility: Expert
Selected by: BslPeriodicSignalSelector
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslPeriodicSignalSourceEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.BslPeriodicSignalSourceEnum | Initializes a new instance of the PLCamera.BslPeriodicSignalSourceEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
DeviceClock | The camera is synchronized via the device clock. Applies to: ace 2 GigE | |
名前 | The full name of BslPeriodicSignalSource (Overrides ParameterListEnum.Name.) | |
PtpClock | The camera is synchronized via the PTP clock. Applies to: ace 2 GigE |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of BslPeriodicSignalSource (Overrides Object.ToString()()()().) |
PLCamera.BslPeriodicSignalSourceEnum.ToString Method#
The full name of BslPeriodicSignalSource
Return Value#
Type: String
Returns the full name of BslPeriodicSignalSource
PLCamera.BslPeriodicSignalSourceEnum Constructor#
Initializes a new instance of the PLCamera.BslPeriodicSignalSourceEnum class
PLCamera.BslPeriodicSignalSourceEnum.DeviceClock Property#
The camera is synchronized via the device clock.
Applies to: ace 2 GigE
PLCamera.BslPeriodicSignalSourceEnum.Name Property#
The full name of BslPeriodicSignalSource
PLCamera.BslPeriodicSignalSourceEnum.PtpClock Property#
The camera is synchronized via the PTP clock.
Applies to: ace 2 GigE