PLCamera.BslSensorBitDepthEnum Class#
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslSensorBitDepthEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLCamera.BslSensorBitDepthEnum | Initializes a new instance of the PLCamera.BslSensorBitDepthEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
Bpp10 | The sensor bit depth is set to 10 bits per pixel. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Bpp12 | The sensor bit depth is set to 12 bits per pixel. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
Bpp8 | The sensor bit depth is set to 8 bits per pixel. Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB | |
名前 | The full name of BslSensorBitDepth (Overrides ParameterListEnum.Name.) |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of BslSensorBitDepth (Overrides Object.ToString()()()().) |
PLCamera.BslSensorBitDepthEnum.ToString Method#
The full name of BslSensorBitDepth
Return Value#
Type: String
Returns the full name of BslSensorBitDepth
PLCamera.BslSensorBitDepthEnum Constructor#
Initializes a new instance of the PLCamera.BslSensorBitDepthEnum class
PLCamera.BslSensorBitDepthEnum.Bpp10 Property#
The sensor bit depth is set to 10 bits per pixel.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.BslSensorBitDepthEnum.Bpp12 Property#
The sensor bit depth is set to 12 bits per pixel.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.BslSensorBitDepthEnum.Bpp8 Property#
The sensor bit depth is set to 8 bits per pixel.
Applies to: ace 2 GigE, ace 2 USB, boost CoaXPress and dart 2 USB
PLCamera.BslSensorBitDepthEnum.Name Property#
The full name of BslSensorBitDepth