PLTransportLayer.TriggerInSourceEnum Class#
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLTransportLayer.TriggerInSourceEnum
Constructors#
名前 | 説明 | |
---|---|---|
PLTransportLayer.TriggerInSourceEnum | Initializes a new instance of the PLTransportLayer.TriggerInSourceEnum class |
プロパティ#
名前 | 説明 | |
---|---|---|
GPITriggerSource0 | GPI Trigger Source 0 Applies to: CoaXPress | |
GPITriggerSource1 | GPI Trigger Source 1 Applies to: CoaXPress | |
GPITriggerSource2 | GPI Trigger Source 2 Applies to: CoaXPress | |
GPITriggerSource3 | GPI Trigger Source 3 Applies to: CoaXPress | |
GPITriggerSource4 | GPI Trigger Source 4 Applies to: CoaXPress | |
GPITriggerSource5 | GPI Trigger Source 5 Applies to: CoaXPress | |
GPITriggerSource6 | GPI Trigger Source 6 Applies to: CoaXPress | |
GPITriggerSource7 | GPI Trigger Source 7 Applies to: CoaXPress | |
名前 | The full name of TriggerInSource (Overrides ParameterListEnum.Name.) | |
TriggerInSourceFrontGPI0 | The trigger input source is set to TriggerInSourceFrontGPI0. Applies to: CoaXPress | |
TriggerInSourceFrontGPI1 | The trigger input source is set to TriggerInSourceFrontGPI1. Applies to: CoaXPress | |
TriggerInSourceFrontGPI2 | The trigger input source is set to TriggerInSourceFrontGPI2. Applies to: CoaXPress | |
TriggerInSourceFrontGPI3 | The trigger input source is set to TriggerInSourceFrontGPI3. Applies to: CoaXPress |
方法#
名前 | 説明 | |
---|---|---|
ToString | The full name of TriggerInSource (Overrides Object.ToString()()()().) |
PLTransportLayer.TriggerInSourceEnum.ToString Method#
The full name of TriggerInSource
Return Value#
Type: String
Returns the full name of TriggerInSource
PLTransportLayer.TriggerInSourceEnum Constructor#
Initializes a new instance of the PLTransportLayer.TriggerInSourceEnum class
PLTransportLayer.TriggerInSourceEnum.GPITriggerSource0 Property#
GPI Trigger Source 0
Applies to: CoaXPress
PLTransportLayer.TriggerInSourceEnum.GPITriggerSource1 Property#
GPI Trigger Source 1
Applies to: CoaXPress
PLTransportLayer.TriggerInSourceEnum.GPITriggerSource2 Property#
GPI Trigger Source 2
Applies to: CoaXPress
PLTransportLayer.TriggerInSourceEnum.GPITriggerSource3 Property#
GPI Trigger Source 3
Applies to: CoaXPress
PLTransportLayer.TriggerInSourceEnum.GPITriggerSource4 Property#
GPI Trigger Source 4
Applies to: CoaXPress
PLTransportLayer.TriggerInSourceEnum.GPITriggerSource5 Property#
GPI Trigger Source 5
Applies to: CoaXPress
PLTransportLayer.TriggerInSourceEnum.GPITriggerSource6 Property#
GPI Trigger Source 6
Applies to: CoaXPress
PLTransportLayer.TriggerInSourceEnum.GPITriggerSource7 Property#
GPI Trigger Source 7
Applies to: CoaXPress
PLTransportLayer.TriggerInSourceEnum.Name Property#
The full name of TriggerInSource
PLTransportLayer.TriggerInSourceEnum.TriggerInSourceFrontGPI0 Property#
The trigger input source is set to TriggerInSourceFrontGPI0.
Applies to: CoaXPress
PLTransportLayer.TriggerInSourceEnum.TriggerInSourceFrontGPI1 Property#
The trigger input source is set to TriggerInSourceFrontGPI1.
Applies to: CoaXPress
PLTransportLayer.TriggerInSourceEnum.TriggerInSourceFrontGPI2 Property#
The trigger input source is set to TriggerInSourceFrontGPI2.
Applies to: CoaXPress
PLTransportLayer.TriggerInSourceEnum.TriggerInSourceFrontGPI3 Property#
The trigger input source is set to TriggerInSourceFrontGPI3.
Applies to: CoaXPress