GenApiノードのインターフェースとアクセスモードチェック機能#
ファイル#
名前 |
---|
GenApi/GenApi.h Main include file for using GenApi with smart pointers. |
GenApi/IBase.h Definition of interface IBase. |
GenApi/IBoolean.h Definition of IBoolean interface. |
GenApi/ICategory.h Definition of interface ICategory and types FeatureList_t : |
GenApi/ICommand.h Definition of ICommand interface. |
GenApi/IEnumEntry.h |
GenApi/IEnumeration.h Definition of interface IEnumeration. |
GenApi/IEnumerationT.h Definition of interface IEnumerationT. |
GenApi/IFloat.h Definition of the IFloat interface. |
GenApi/IInteger.h Definition of the interface IInteger. |
GenApi/INode.h Definition of interface INode and types NodeList_t and CallbackHandleType: |
GenApi/INodeMap.h Definition of interface INodeMap. |
GenApi/IPort.h Definition of interface IPort. |
GenApi/IRegister.h Definition of RegisterList_t type and the interface IRegister. |
GenApi/IString.h Definition of interface IString. |
GenApi/IValue.h Definition of the interface IValue. |
GenApi/NodeMapRef.h Definition of CNodeMapRef. |
クラス#
名前 | |
---|---|
struct | GenApi::IBase Base interface common to all nodes. |
struct | GenApi::IBoolean Interface for Boolean properties. |
struct | GenApi::ICategory Gives access to a category node. |
struct | GenApi::ICommand |
struct | GenApi::IEnumEntry Interface of single enum value. |
struct | GenApi::IEnumeration Interface for enumeration properties. |
struct | GenApi::IEnumerationT Interface for enumeration properties. |
struct | GenApi::IFloat Interface for float properties. |
struct | GenApi::IInteger Interface for integer properties. |
struct | GenApi::INode Interface common to all nodes. |
struct | GenApi::INodeMap Interface to access the node map. |
struct | GenApi::IPort Interface for ports. |
struct | GenApi::IRegister Interface for registers. |
struct | GenApi::IString Interface for string properties. |
struct | GenApi::IValue Interface for value properties. |
class | GenApi::CNodeMapRefT Smartpointer template for NodeMaps with create function. |
class | GenApi::CGeneric_XMLLoaderParams Empty base class used by class CNodeMapRef as generic template argument. |
class | GenApi::CNodeMapRef Smartpointer for NodeMaps with create function. |
Functions#
名前 | |
---|---|
bool | IsReadable(EAccessMode AccessMode) Tests if readable. |
bool | IsReadable(const IBase * p) Checks if a node is readable. |
bool | IsReadable(const IBase & r) Checks if a node is readable. |
bool | IsWritable(EAccessMode AccessMode) Tests if writable. |
bool | IsWritable(const IBase * p) Checks if a node is writable. |
bool | IsWritable(const IBase & r) Checks if a node is writable. |
bool | IsImplemented(EAccessMode AccessMode) Tests if implemented. |
bool | IsImplemented(const IBase * p) Checks if a node is implemented. |
bool | IsImplemented(const IBase & r) Checks if a node is implemented. |
bool | IsAvailable(EAccessMode AccessMode) Tests if available. |
bool | IsAvailable(const IBase * p) Checks if a node is available. |
bool | IsAvailable(const IBase & r) Checks if a node is available. |
EAccessMode | Combine(EAccessMode Peter, EAccessMode Paul) Computes which access mode the two guards allow together. |
bool | IsVisible(EVisibility Visibility, EVisibility MaxVisiblity) Tests Visibility. |
EVisibility | Combine(EVisibility Peter, EVisibility Paul) Computes which visibility the two guards allow together. |
bool | IsCacheable(ECachingMode CachingMode) Tests Cacheability. |
ECachingMode | Combine(ECachingMode Peter, ECachingMode Paul) Computes which CachingMode results from a combination. |
Functions Documentation#
function IsReadable#
Tests if readable.
function IsReadable#
Checks if a node is readable.
function IsReadable#
Checks if a node is readable.
function IsWritable#
Tests if writable.
function IsWritable#
Checks if a node is writable.
function IsWritable#
Checks if a node is writable.
function IsImplemented#
Tests if implemented.
function IsImplemented#
Checks if a node is implemented.
function IsImplemented#
Checks if a node is implemented.
function IsAvailable#
Tests if available.
function IsAvailable#
Checks if a node is available.
function IsAvailable#
Checks if a node is available.
function Combine#
Computes which access mode the two guards allow together.
function IsVisible#
Tests Visibility.
CAVE : this relys on the EVisibility enum's coding
function Combine#
Computes which visibility the two guards allow together.
function IsCacheable#
Tests Cacheability.
function Combine#
Computes which CachingMode results from a combination.