IImage Interface#
Syntax#
C#
VB
The IImage type exposes the following members.
プロパティ#
名前 | 説明 | |
---|---|---|
Height | The height of the image in pixels, i.e. the number of image rows. | |
IsValid | Indicates if the image is valid. | |
Orientation | The vertical orientation of the pixel data stored in memory. | |
PaddingX | The number of data bytes added to the end of each row. | |
PixelData | The pixel data buffer. The type of the object containing the buffer depends on the class implementing this interface. The pixel data buffer is provided as a byte array if no custom buffer factory is used. With a custom buffer factory the provided type is dependent on its specific implementation. | |
PixelDataPointer | The pointer to the pixel data buffer. | |
PixelTypeValue | The pixel type. | |
Width | The width of the image in pixels, i.e. the number of image columns. |
Extension Methods#
名前 | 説明 | |
---|---|---|
ComputeStride | Computes the stride of the image in bytes. Returns null if the stride cannot be computed. (Defined by IImageExtensions.) | |
画面 | Uses the ImageWindow method DisplayImage(Int32, IImage) to display the image. (Defined by IImageExtensions.) |
IImage.Height Property#
The height of the image in pixels, i.e. the number of image rows.
Syntax#
C#
VB
Property Value#
Type: Int32
Remarks#
Error Safety: Does not throw exceptions.
IImage.IsValid Property#
Indicates if the image is valid.
Syntax#
C#
VB
Return Value#
Type: Boolean
Returns true if the image is valid.
Remarks#
IImage.Orientation Property#
The vertical orientation of the pixel data stored in memory.
Syntax#
C#
VB
Property Value#
Type: ImageOrientation
Remarks#
Error Safety: Does not throw exceptions.
IImage.PaddingX Property#
The number of data bytes added to the end of each row.
Syntax#
C#
VB
Property Value#
Type: Int32
Remarks#
Error Safety: Does not throw exceptions.
IImage.PixelData Property#
The pixel data buffer. The type of the object containing the buffer depends on the class implementing this interface. The pixel data buffer is provided as a byte array if no custom buffer factory is used. With a custom buffer factory the provided type is dependent on its specific implementation.
Syntax#
C#
VB
Property Value#
Type: Object
Remarks#
Error Safety: Does not throw exceptions.
IImage.PixelDataPointer Property#
The pointer to the pixel data buffer.
Syntax#
C#
VB
Property Value#
Type: IntPtr
Remarks#
Error Safety: Does not throw exceptions.
IImage.PixelTypeValue Property#
The pixel type.
Syntax#
C#
VB
Property Value#
Type: PixelType
Remarks#
Error Safety: Does not throw exceptions.
IImage.Width Property#
The width of the image in pixels, i.e. the number of image columns.
Syntax#
C#
VB
Property Value#
Type: Int32
Remarks#
Error Safety: Does not throw exceptions.