コンテンツにスキップ
STAGING SERVER
DEVELOPMENT SERVER

System Integration#

This topic provides information regarding optimum installation conditions.

Use outside of the specified conditions could cause the device to fail and/or function incorrectly. These conditions are applicable for the environment immediately around the device under all operational conditions. When used with an external enclosure, active temperature control and/or other cooling solutions are recommended to ensure the device is maintained within these ranges.

Installation Recommendations#

  1. When using an external housing around the camera for dust-proofing, use foam inserts or rubber gaskets between the front of the camera and the external housing.
  2. Avoid external forces applied to the camera chassis during the installation process.
  3. Disassembling the chassis voids the warranty.
  4. For a detailed installation reference solution, see the Reference Design: Mounting Stereo mini USB Cameras topic.

熱放散対策#

  1. Avoid direct heat sources in close proximity to the camera.
  2. Providing more space inside the external housing may help to lower the operating temperature.
  3. For a detailed heat dissipation reference solution, see the Reference Design: Thermal Best Practices topic.

Cable Design Guide#

  1. Basler recommends using a 1-m USB Type-C cable. If a longer cable is required, select a USB-IF certified cable that supports both power and data (≥3.0 m length is recommended).
  2. For detailed cable design guidance, see the Reference Design: USB Cable topic.