コンテンツにスキップ
STAGING SERVER
DEVELOPMENT SERVER

Cautions#

  • Follow the instructions carefully when operating the camera. Improper handling may lead to damage to the internal components.
  • Do not drop the camera or expose the camera to mechanical stress.
  • Do not attempt to modify the camera as such modifications may cause permanent damage or performance degradation.
  • The temperature of the camera may rise during long periods of use.
  • Do not touch the lens. Fingerprints on the lens may affect image quality.
  • Keep the product beyond the reach of children or animals to avoid accidents.
  • If the computer does not recognize the camera, verify that the cable meets the power and data transfer requirements, then replug it into the USB port to reconnect.
  • This product is classified as a Class 1 Laser Product under the international standard Class 1, EN IEC 60825-1:2007 Edition 2, EN IEC 60825-1:2014 Edition 3. Using controls, adjustments, or procedures other than those specified herein may result in hazardous radiation exposure.

Safety and Handling Instructions#

  • Avoid powering on the product if any external damage was observed.
  • Do not attempt to open any portion of this product. There are no user serviceable parts.
  • Be cautious of invisible laser radiation. Avoid direct exposure to the beam.
  • To maintain compliance and safety standards, do not modify or service the product. Unauthorized modifications or servicing could result in emissions surpassing the Class 1 safety level.
  • Only update the camera firmware with official releases that match the specific module SKU and revision to ensure proper functionality and safety.