Auto Function Profile (dart E)#
機能を使用する#
Auto Function Profileの設定#
オートファンクションプロファイルを設定するには次の手順を実行します。
- パラメーターを Gain Auto auto function and the Exposure Auto 自動機能の適用先:
Continuous. - パラメーターを
AutoFunctionProfileパラメーターを次のいずれかの値に設定します。AntiFlicker50Hz: 50 Hzの電源周波数に対するフリッカー低減を有効にします(ヨーロッパなどに適用されます)。AntiFlicker60Hz: 60 Hzの電源周波数に対するフリッカー低減を有効にします(北米などに適用されます)。AntiFlickerAuto: 電源周波数の自動検出によるフリッカー低減を有効にします。MinimizeExposureTime: 自動調整プロセス中、Exposure Timeは可能な限り低く抑えられます。MinimizeGain(デフォルト): 自動調整プロセス中、ゲインは可能な限り低く抑えられます。
サンプルコード#
// Set the auto function profile to Minimize Gain
camera.AutoFunctionProfile.SetValue(AutoFunctionProfile_MinimizeGain);
// Set the auto function profile to Minimize Exposure Time
camera.AutoFunctionProfile.SetValue(AutoFunctionProfile_MinimizeExposureTime);
// Enable Gain and Exposure Auto auto functions and set the operating mode to Continuous
camera.GainAuto.SetValue(GainAuto_Continuous);
camera.ExposureAuto.SetValue(ExposureAuto_Continuous);
INodeMap& nodemap = camera.GetNodeMap();
// Set the auto function profile to Minimize Gain
CEnumParameter(nodemap, "AutoFunctionProfile").SetValue("MinimizeGain");
// Set the auto function profile to Minimize Exposure Time
CEnumParameter(nodemap, "AutoFunctionProfile").SetValue("MinimizeExposureTime");
// Enable Gain and Exposure Auto auto functions and set the operating mode to Continuous
CEnumParameter(nodemap, "GainAuto").SetValue("Continuous");
CEnumParameter(nodemap, "ExposureAuto").SetValue("Continuous");
// Set the auto function profile to Minimize Gain
camera.Parameters[PLCamera.AutoFunctionProfile].SetValue(PLCamera.AutoFunctionProfile.MinimizeGain);
// Set the auto function profile to Minimize Exposure Time
camera.Parameters[PLCamera.AutoFunctionProfile].SetValue(PLCamera.AutoFunctionProfile.MinimizeExposureTime);
// Enable Gain and Exposure Auto auto functions and set the operating mode to Continuous
camera.Parameters[PLCamera.GainAuto].SetValue(PLCamera.GainAuto.Continuous);
camera.Parameters[PLCamera.ExposureAuto].SetValue(PLCamera.ExposureAuto.Continuous);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
/* Set the auto function profile to Minimize Gain */
errRes = PylonDeviceFeatureFromString(hdev, "AutoFunctionProfile", "MinimizeGain");
CHECK(errRes);
/* Set the auto function profile to Minimize Exposure Time */
errRes = PylonDeviceFeatureFromString(hdev, "AutoFunctionProfile", "MinimizeExposureTime");
CHECK(errRes);
/* Enable Gain and Exposure Auto auto functions and set the operating mode to Continuous */
errRes = PylonDeviceFeatureFromString(hdev, "GainAuto", "Continuous");
CHECK(errRes);
errRes = PylonDeviceFeatureFromString(hdev, "ExposureAuto", "Continuous");
CHECK(errRes);
# Set the auto function profile to Minimize Gain
camera.AutoFunctionProfile.Value = "MinimizeGain"
# Set the auto function profile to Minimize Exposure Time
camera.AutoFunctionProfile.Value = "MinimizeExposureTime"
# Enable Gain and Exposure Auto auto functions and set the operating mode to Continuous
camera.GainAuto.Value = "Continuous"
camera.ExposureAuto.Value = "Continuous"
pylon Viewer を使用してパラメータを簡単に設定することもできます。