カメラの取り付け#
Basler ace/ace 2 USB 3.0, dart USB 3.0, and pulse USB 3.0 Cameras#
To install a Basler ace/ace 2 USB 3.0, dart USB 3.0, or pulse USB 3.0 camera on a Windows computer, complete the installation process in the following order:
Basler ace/ace 2 GigE, dart M GigE, and racer 2 GigE Cameras#
To install a Basler ace/ace 2 GigE, dart M, or a racer 2 GigE camera on a Windows computer, complete the installation process in the following order:
- ソフトウェアのインストール(Windows)
- ハードウェアのインストール(GigEカメラ)
- ネットワークの設定(GigEカメラ)
- オプション:「ワイヤレスLANでBasler GigEカメラを使用する」
Basler ace 2 GMSL Cameras#
To install and configure a Basler ace 2 GMSL camera on a Linux system, complete the installation process in the following order:
- ソフトウェアのインストール(Linux)
- Installation Camera Enablement Package (GMSL Cameras)
- Hardware Installation (GMSL Cameras)
- Configuring Basler GMSL Cameras
Basler CoaXPress Cameras#
Depending on whether you want to install a Basler CoaXPress camera on a Windows computer or on a Linux system, complete the installation process in the following order:
Further Information#
- To set up a racer 2 S or racer 2 L line scan camera with a frame grabber or an interface card, refer to the Configuring CXP Line Scan Cameras and Frame Grabbers section.
- To set up a racer 2 XL line scan camera with a frame grabber, refer to the Configuring a CoaXPress-over-Fiber System section.