Multi-Camera Systems#
Multi-camera setups are common in industrial applications such as inspection, 3D reconstruction, and synchronized data acquisition. They are used when a single camera isn't sufficient to capture all the required information.
Typical use cases:
- Capturing different viewpoints of an object
- Increasing the field of view
- Increasing throughput
- Parallel inspection of multiple objects
Fundamental Challenges#
Working with multiple cameras introduces several challenges:
- Synchronization (timing)
- Bandwidth limitations (especially when using GigE cameras)
- CPU load (processing multiple streams)
- Device identification and mapping
Device Identification#
Each camera must have a unique identifier, typically its serial number.
Mapping example:
Avoid using indices such as devices[0] because the order in which cameras are enumerated may change. For more details, see Enumerating Cameras.
Creating Multiple Camera Instances#
from pypylon import pylon
factory = pylon.TlFactory.GetInstance()
device_info_list = factory.EnumerateDevices()
cameras = []
for device_info in device_info_list:
camera = pylon.InstantCamera(factory.CreateDevice(device_info))
camera.Open()
cameras.append(camera)
This creates and opens one camera instance per device.
Acquisition Methods#
When using multiple cameras, you have to decide on an acquisition method: sequential or parallel.
Sequential Acquisition#
This means that image processing is done one camera after the other.
Key characteristics of this method:
- Simple to implement
- Not time-synchronized
- Slower overall
Parallel Acquisition#
This means that images from several cameras are processed together.
Key characteristics of this method:
- Cameras acquire simultaneously
- Required for synchronization
- Higher CPU and bandwidth requirements
Synchronization Methods#
To synchronize cameras, you can choose between software and hardware synchronization. The advantages and disadvantages are similar to software vs. hardware triggering.
Software Synchronization#
Key characteristics of this method:
- Trigger cameras via software
- Limited precision
- Affected by operating system scheduling
例:
Hardware Synchronization (Recommended)#
Key characteristics of this method:
- Precise timing
- Deterministic behavior
- Required for stereo or measurement systems
Bandwidth Considerations (GigE)#
Multiple GigE cameras share the same network bandwidth.
Potential problems:
- Packet loss
- Dropped frames
- Increased latency
You can use one of the following strategies to mitigate potential problems:
- Use dedicated network interface cards (NICs)
- Enable jumbo frames (MTU 9000)
- Reduce ROI or frame rate
- Configure packet delay
Processing Architecture#
Single-Threaded#
- Simple
- Limited scalability
Multi-Threaded (Recommended)#
- Scalable
- Better CPU utilization
- More complex to implement
Example Patterns#
Basic Multi-Camera Loop (Sequential Polling)#
from pypylon import pylon
def process(image):
print(image.shape)
factory = pylon.TlFactory.GetInstance()
device_info_list = factory.EnumerateDevices()
cameras = [pylon.InstantCamera(factory.CreateDevice(device_info)) for device_info in device_info_list]
for camera in cameras:
camera.Open()
camera.StartGrabbing()
while any(camera.IsGrabbing() for camera in cameras):
for camera in cameras:
if camera.IsGrabbing():
with camera.RetrieveResult(1000) as grab_result:
if grab_result.GrabSucceeded():
image = grab_result.Array
# Do processing on image here, e.g. call a function.
process(image)
Advanced Approach: InstantCameraArray (Recommended)#
pypylon provides a dedicated abstraction for multi-camera setups: InstantCameraArray.
This class manages multiple cameras and provides a single unified RetrieveResult() call, including information about which camera delivered the image.
from pypylon import pylon
def process(image):
print(image.shape)
COUNT_OF_IMAGES_TO_GRAB = 100
RETRIEVE_TIMEOUT_MS = 5000
factory = pylon.TlFactory.GetInstance()
device_info_list = factory.EnumerateDevices()
with pylon.InstantCameraArray(len(device_info_list)) as cameras:
for i, camera in enumerate(cameras):
camera.Attach(factory.CreateDevice(device_info_list[i]))
print("Using device:", camera.DeviceInfo.ModelName)
cameras.StartGrabbing()
for i in range(COUNT_OF_IMAGES_TO_GRAB):
if not cameras.IsGrabbing():
break
with cameras.RetrieveResult(
RETRIEVE_TIMEOUT_MS,
pylon.TimeoutHandling_ThrowException
) as grab_result:
if grab_result.GrabSucceeded():
cam_idx = grab_result.CameraContext
print(f"Camera {cam_idx}: {cameras[cam_idx].DeviceInfo.ModelName}")
image = grab_result.Array
# Do processing on image here, e.g. call a function.
process(image)
else:
print("Error:", grab_result.ErrorDescription)
Why InstantCameraArray Is Important
Compared to manual looping, this approach provides:
- single acquisition loop for all cameras
- automatic camera context tracking (
camera.CameraContext) - simpler synchronization handling
- more efficient thread usage
Conceptually:
Practical Design Guidelines#
- Always identify cameras by serial number.
- Prefer hardware synchronization.
- Reduce bandwidth where possible (e.g., by specifying a ROI or lowering the frame rate).
- Use separate processing threads for scalability.
- Monitor system load (CPU, network).
Common Pitfalls#
- Relying on device index.
- Exceeding network bandwidth.
- Ignoring synchronization requirements.
- Blocking processing in acquisition loop.
Mental Model#
Key Takeaways#
- Multi-camera systems require careful design.
- Synchronization is critical for many applications.
- Bandwidth and CPU must be considered early.
- Scalable architectures use parallel processing.