Skip to content
STAGING SERVER

PLCamera.BLCSerialTransmitQueueStatusEnum Class#

Reports the status of the serial communication transmit queue.

Applies to: ace GigE and ace USB

Visibility: Guru

The feature documentation may provide more information.

Inheritance Hierarchy#

System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLCamera.BLCSerialTransmitQueueStatusEnum

Constructors#

 NameDescription
Public methodPLCamera.BLCSerialTransmitQueueStatusEnum Initializes a new instance of the PLCamera.BLCSerialTransmitQueueStatusEnum class
 

Properties#

 NameDescription
Public propertyEmpty

The transmit queue is empty.

Applies to: ace GigE and ace USB

Public propertyFilled

The transmit queue contains at least one value.

Applies to: ace GigE and ace USB

Public propertyFull

The transmit queue is full.

Applies to: ace GigE and ace USB

Public propertyName The full name of BLCSerialTransmitQueueStatus (Overrides ParameterListEnum.Name.)
 

Methods#

 NameDescription
Public methodToString The full name of BLCSerialTransmitQueueStatus (Overrides Object.ToString()()()().)
 

PLCamera.BLCSerialTransmitQueueStatusEnum.ToString Method#

The full name of BLCSerialTransmitQueueStatus

Return Value#

Type: String
Returns the full name of BLCSerialTransmitQueueStatus

PLCamera.BLCSerialTransmitQueueStatusEnum Constructor#

Initializes a new instance of the PLCamera.BLCSerialTransmitQueueStatusEnum class

PLCamera.BLCSerialTransmitQueueStatusEnum.Empty Property#

The transmit queue is empty.

Applies to: ace GigE and ace USB

PLCamera.BLCSerialTransmitQueueStatusEnum.Filled Property#

The transmit queue contains at least one value.

Applies to: ace GigE and ace USB

PLCamera.BLCSerialTransmitQueueStatusEnum.Full Property#

The transmit queue is full.

Applies to: ace GigE and ace USB

PLCamera.BLCSerialTransmitQueueStatusEnum.Name Property#

The full name of BLCSerialTransmitQueueStatus