Skip to content

StringName Structure#

Defines a string parameter name by combining the parameter name string and the parameter type information.

Syntax#

C#

public struct StringName

VB

Public Structure StringName

The StringName type exposes the following members.

Constructors#

NameDescription
Public methodStringName Creates a string parameter name.
 

Properties#

NameDescription
Public propertyName The string parameter name as string.
 

Methods#

NameDescription
Public methodToString The string parameter name as string. (Overrides ValueType.ToString().)
 

Operators#

NameDescription
Public operatorStatic memberExplicit(String to StringName) Creates a string parameter name from a string.
 

StringName Explicit Conversion (String to StringName)#

Creates a string parameter name from a string.

Syntax#

C#

public static explicit operator StringName (
    string name
)

VB

Public Shared Narrowing Operator CType ( 
    name As String
) As StringName

Parameters#

 

name
Type: System.String
The name of the parameter as string. The name can include path information.

Return Value#

Type: StringName
Returns the string parameter name.

StringName.ToString Method#

The string parameter name as string.

Syntax#

C#

public override sealed string ToString()

VB

Public Overrides NotOverridable Function ToString As String

Return Value#

Type: String
Returns the string parameter name as string. The name can include path information.

StringName Constructor#

Creates a string parameter name.

Syntax#

C#

public StringName(
    string name
)

VB

Public Sub New ( 
    name As String
)

Parameters#

 

name
Type: System.String
The name of the parameter as string. The name can include path information.

StringName.Name Property#

The string parameter name as string.

Syntax#

C#

public string Name { get; }

VB

Public ReadOnly Property Name As String
    Get

Property Value#

Type: String

StringName Type Conversions#

The StringName type exposes the following members.

Operators#

NameDescription
Public operatorStatic memberExplicit(String to StringName) Creates a string parameter name from a string.