Skip to content

PLCamera.GevStreamChannelSelectorEnum Class#

Sets the stream channels to be configured. All changes to the stream channel settings will be applied to the selected stream channel.

Applies to: GigE

Visibility: Guru

Selecting Parameters: GevGVSPExtendedIDMode, GevSCBWA, GevSCBWR, GevSCBWRA, GevSCDA, GevSCDCT, GevSCDMT, GevSCFJM, GevSCFTD, GevSCPD, GevSCPHostPort, GevSCPInterfaceIndex, GevSCPSBigEndian, GevSCPSDoNotFragment, GevSCPSFireTestPacket, GevSCPSPacketSize

The feature documentation may provide more information.

Inheritance Hierarchy#

System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLCamera.GevStreamChannelSelectorEnum

Constructors#

 NameDescription
Public methodPLCamera.GevStreamChannelSelectorEnum Initializes a new instance of the PLCamera.GevStreamChannelSelectorEnum class
 

Properties#

 NameDescription
Public propertyName The full name of GevStreamChannelSelector (Overrides ParameterListEnum.Name.)
Public propertyStreamChannel0

Stream channel 0 can be configured.

Applies to: GigE

 

Methods#

 NameDescription
Public methodToString The full name of GevStreamChannelSelector (Overrides Object.ToString()()()().)
 

PLCamera.GevStreamChannelSelectorEnum.ToString Method#

The full name of GevStreamChannelSelector

Return Value#

Type: String
Returns the full name of GevStreamChannelSelector

PLCamera.GevStreamChannelSelectorEnum Constructor#

Initializes a new instance of the PLCamera.GevStreamChannelSelectorEnum class

PLCamera.GevStreamChannelSelectorEnum.Name Property#

The full name of GevStreamChannelSelector

PLCamera.GevStreamChannelSelectorEnum.StreamChannel0 Property#

Stream channel 0 can be configured.

Applies to: GigE