Skip to content
STAGING SERVER

PLVideoWriter.CompressionModeEnum Class#

Sets the compression mode. You can choose whether to keep the bit rate or the quality of the resulting video stream constant.

Visibility: Beginner

Inheritance Hierarchy#

System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLVideoWriter.CompressionModeEnum

Constructors#

 NameDescription
Public methodPLVideoWriter.CompressionModeEnum Initializes a new instance of the PLVideoWriter.CompressionModeEnum class
 

Properties#

 NameDescription
Public propertyBitrate

The resulting stream has a constant bit rate.

Public propertyName The full name of CompressionMode (Overrides ParameterListEnum.Name.)
Public propertyQuality

The resulting stream has a constant quality.

 

Methods#

 NameDescription
Public methodToString The full name of CompressionMode (Overrides Object.ToString()()()().)
 

PLVideoWriter.CompressionModeEnum.ToString Method#

The full name of CompressionMode

Return Value#

Type: String
Returns the full name of CompressionMode

PLVideoWriter.CompressionModeEnum Constructor#

Initializes a new instance of the PLVideoWriter.CompressionModeEnum class

PLVideoWriter.CompressionModeEnum.Bitrate Property#

The resulting stream has a constant bit rate.

PLVideoWriter.CompressionModeEnum.Name Property#

The full name of CompressionMode

PLVideoWriter.CompressionModeEnum.Quality Property#

The resulting stream has a constant quality.