PLCamera.TriggerDelaySourceEnum Class#
Applies to: CameraLink and GigE
Visibility: Expert
Selected by: TriggerSelector
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.TriggerDelaySourceEnum
Constructors#
Name | Description | |
---|---|---|
![]() | PLCamera.TriggerDelaySourceEnum | Initializes a new instance of the PLCamera.TriggerDelaySourceEnum class |
Properties#
Name | Description | |
---|---|---|
![]() | LineTrigger | The trigger delay is expressed as a number of line triggers. Applies to: CameraLink and GigE |
![]() | Name | The full name of TriggerDelaySource (Overrides ParameterListEnum.Name.) |
![]() | Time_us | The trigger delay is expressed as a time interval in microseconds. Applies to: CameraLink and GigE |
Methods#
Name | Description | |
---|---|---|
![]() | ToString | The full name of TriggerDelaySource (Overrides Object.ToString()()()().) |
PLCamera.TriggerDelaySourceEnum.ToString Method#
The full name of TriggerDelaySource
Return Value#
Type: String
Returns the full name of TriggerDelaySource
PLCamera.TriggerDelaySourceEnum Constructor#
Initializes a new instance of the PLCamera.TriggerDelaySourceEnum class
PLCamera.TriggerDelaySourceEnum.LineTrigger Property#
The trigger delay is expressed as a number of line triggers.
Applies to: CameraLink and GigE
PLCamera.TriggerDelaySourceEnum.Name Property#
The full name of TriggerDelaySource
PLCamera.TriggerDelaySourceEnum.Time_us Property#
The trigger delay is expressed as a time interval in microseconds.
Applies to: CameraLink and GigE