PLCamera.BslTwiTransferStatusEnum Class#
Applies to: dart 2 USB
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BslTwiTransferStatusEnum
Constructors#
Name | Description | |
---|---|---|
PLCamera.BslTwiTransferStatusEnum | Initializes a new instance of the PLCamera.BslTwiTransferStatusEnum class |
Properties#
Name | Description | |
---|---|---|
NakAddress | The last transfer failed because a NAK was received when sending the address. Applies to: dart 2 USB | |
NakData | The last transfer failed because a NAK was received when sending data. Applies to: dart 2 USB | |
Name | The full name of BslTwiTransferStatus (Overrides ParameterListEnum.Name.) | |
Pending | A transfer is pending. Applies to: dart 2 USB | |
Success | The last transfer was successful. Applies to: dart 2 USB |
Methods#
Name | Description | |
---|---|---|
ToString | The full name of BslTwiTransferStatus (Overrides Object.ToString()()()().) |
PLCamera.BslTwiTransferStatusEnum.ToString Method#
The full name of BslTwiTransferStatus
Return Value#
Type: String
Returns the full name of BslTwiTransferStatus
PLCamera.BslTwiTransferStatusEnum Constructor#
Initializes a new instance of the PLCamera.BslTwiTransferStatusEnum class
PLCamera.BslTwiTransferStatusEnum.NakAddress Property#
The last transfer failed because a NAK was received when sending the address.
Applies to: dart 2 USB
PLCamera.BslTwiTransferStatusEnum.NakData Property#
The last transfer failed because a NAK was received when sending data.
Applies to: dart 2 USB
PLCamera.BslTwiTransferStatusEnum.Name Property#
The full name of BslTwiTransferStatus
PLCamera.BslTwiTransferStatusEnum.Pending Property#
A transfer is pending.
Applies to: dart 2 USB
PLCamera.BslTwiTransferStatusEnum.Success Property#
The last transfer was successful.
Applies to: dart 2 USB