Skip to content
STAGING SERVER
DEVELOPMENT SERVER

PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum Class#

Sets which x coordinate entry can be configured.

Applies to: boost V CoaXPress

Visibility: Expert

Selecting Parameters: BslStaticDefectPixelCorrectionXCoordinate

The feature documentation may provide more information.

Inheritance Hierarchy#

System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum

Constructors#

 NameDescription
Public methodPLCamera.BslStaticDefectPixelCorrectionXSelectorEnum Initializes a new instance of the PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum class
 

Properties#

 NameDescription
Public propertyName The full name of BslStaticDefectPixelCorrectionXSelector (Overrides ParameterListEnum.Name.)
Public propertyX0

Entry X0 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry.

Applies to: boost V CoaXPress

Public propertyX1

Entry X1 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry.

Applies to: boost V CoaXPress

Public propertyX2

Entry X2 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry.

Applies to: boost V CoaXPress

Public propertyX3

Entry X3 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry.

Applies to: boost V CoaXPress

Public propertyX4

Entry X4 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry.

Applies to: boost V CoaXPress

Public propertyX5

Entry X5 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry.

Applies to: boost V CoaXPress

Public propertyX6

Entry X6 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry.

Applies to: boost V CoaXPress

Public propertyX7

Entry X7 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry.

Applies to: boost V CoaXPress

 

Methods#

 NameDescription
Public methodToString The full name of BslStaticDefectPixelCorrectionXSelector (Overrides Object.ToString()()()().)
 

PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum.ToString Method#

The full name of BslStaticDefectPixelCorrectionXSelector

Return Value#

Type: String
Returns the full name of BslStaticDefectPixelCorrectionXSelector

PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum Constructor#

Initializes a new instance of the PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum class

PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum.Name Property#

The full name of BslStaticDefectPixelCorrectionXSelector

PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum.X0 Property#

Entry X0 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry.

Applies to: boost V CoaXPress

PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum.X1 Property#

Entry X1 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry.

Applies to: boost V CoaXPress

PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum.X2 Property#

Entry X2 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry.

Applies to: boost V CoaXPress

PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum.X3 Property#

Entry X3 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry.

Applies to: boost V CoaXPress

PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum.X4 Property#

Entry X4 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry.

Applies to: boost V CoaXPress

PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum.X5 Property#

Entry X5 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry.

Applies to: boost V CoaXPress

PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum.X6 Property#

Entry X6 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry.

Applies to: boost V CoaXPress

PLCamera.BslStaticDefectPixelCorrectionXSelectorEnum.X7 Property#

Entry X7 can be configured. Use the Static Defect Pixel Correction X Coordinate parameter to assign an x coordinate to this entry.

Applies to: boost V CoaXPress