Skip to content

PLCamera.BslSerialNumberOfStopBitsEnum Class#

Sets the number of stop bits used in serial communication.

Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress

Visibility: Expert

The feature documentation may provide more information.

Inheritance Hierarchy#

System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLCamera.BslSerialNumberOfStopBitsEnum

Constructors#

 NameDescription
Public methodPLCamera.BslSerialNumberOfStopBitsEnum Initializes a new instance of the PLCamera.BslSerialNumberOfStopBitsEnum class
 

Properties#

 NameDescription
Public propertyBits1

One stop bit is used in serial communication.

Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress

Public propertyBits2

Two stop bits are used in serial communication.

Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress

Public propertyName The full name of BslSerialNumberOfStopBits (Overrides ParameterListEnum.Name.)
 

Methods#

 NameDescription
Public methodToString The full name of BslSerialNumberOfStopBits (Overrides Object.ToString()()()().)
 

PLCamera.BslSerialNumberOfStopBitsEnum.ToString Method#

The full name of BslSerialNumberOfStopBits

Return Value#

Type: String
Returns the full name of BslSerialNumberOfStopBits

PLCamera.BslSerialNumberOfStopBitsEnum Constructor#

Initializes a new instance of the PLCamera.BslSerialNumberOfStopBitsEnum class

PLCamera.BslSerialNumberOfStopBitsEnum.Bits1 Property#

One stop bit is used in serial communication.

Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress

PLCamera.BslSerialNumberOfStopBitsEnum.Bits2 Property#

Two stop bits are used in serial communication.

Applies to: ace 2 GigE, ace 2 USB and boost CoaXPress

PLCamera.BslSerialNumberOfStopBitsEnum.Name Property#

The full name of BslSerialNumberOfStopBits