ShowMode Enumeration#
Syntax#
C#
VB
Members#
| Member name | Value | Description | |
|---|---|---|---|
| Show | 5 | Shows the image window. | |
| Hide | 0 | Hides the image window. | |
| Maximize | 3 | Maximizes the image window. | |
| Minimize | 6 | Minimizes the image window. | |
| Restore | 9 | Displays the image window. Restores old position and size if the image window was maximized or minimized. | |
| ShowNoActivate | 4 | Shows the image window, but does not activate it. | |
| ForceMinimize | 11 | Minimizes the image window, forces it if needed. | |
| ShowMinimized | 2 | Shows the image window minimized. | |
| ShowMaximized | 3 | Shows the image window maximized. | |
| ShowMinNoActivate | 7 | Shows the image window minimized, but does not activate it. | |
| Normal | 1 | Compatibility with ShowWindow API | |
| ShowNA | 8 | Compatibility with ShowWindow API | |
| ShowDefault | 10 | Compatibility with ShowWindow API |