PLTransportLayer.TriggerOutputEventSelectEnum Class#
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLTransportLayer.TriggerOutputEventSelectEnum
Constructors#
| Name | Description | |
|---|---|---|
|  | PLTransportLayer.TriggerOutputEventSelectEnum | Initializes a new instance of the PLTransportLayer.TriggerOutputEventSelectEnum class | 
Properties#
| Name | Description | |
|---|---|---|
|  | Name | The full name of TriggerOutputEventSelect (Overrides ParameterListEnum.Name.) | 
|  | PulseGenerator0 | The source for the output statistics is set to pulse generator 0. Applies to: CoaXPress | 
|  | PulseGenerator1 | The source for the output statistics is set to pulse generator 1. Applies to: CoaXPress | 
|  | PulseGenerator2 | The source for the output statistics is set to pulse generator 2. Applies to: CoaXPress | 
|  | PulseGenerator3 | The source for the output statistics is set to pulse generator 3. Applies to: CoaXPress | 
Methods#
| Name | Description | |
|---|---|---|
|  | ToString | The full name of TriggerOutputEventSelect (Overrides Object.ToString()()()().) | 
PLTransportLayer.TriggerOutputEventSelectEnum.ToString Method#
The full name of TriggerOutputEventSelect
Return Value#
Type: String
Returns the full name of TriggerOutputEventSelect
PLTransportLayer.TriggerOutputEventSelectEnum Constructor#
Initializes a new instance of the PLTransportLayer.TriggerOutputEventSelectEnum class
PLTransportLayer.TriggerOutputEventSelectEnum.Name Property#
The full name of TriggerOutputEventSelect
PLTransportLayer.TriggerOutputEventSelectEnum.PulseGenerator0 Property#
The source for the output statistics is set to pulse generator 0.
Applies to: CoaXPress
PLTransportLayer.TriggerOutputEventSelectEnum.PulseGenerator1 Property#
The source for the output statistics is set to pulse generator 1.
Applies to: CoaXPress
PLTransportLayer.TriggerOutputEventSelectEnum.PulseGenerator2 Property#
The source for the output statistics is set to pulse generator 2.
Applies to: CoaXPress
PLTransportLayer.TriggerOutputEventSelectEnum.PulseGenerator3 Property#
The source for the output statistics is set to pulse generator 3.
Applies to: CoaXPress