PLTransportLayer.TriggerCameraOutSelectEnum Class#
Applies to: CoaXPress
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLTransportLayer.TriggerCameraOutSelectEnum
Constructors#
| Name | Description | |
|---|---|---|
![]() | PLTransportLayer.TriggerCameraOutSelectEnum | Initializes a new instance of the PLTransportLayer.TriggerCameraOutSelectEnum class |
Properties#
| Name | Description | |
|---|---|---|
![]() | BypassFrontGPI0 | The output source is set to BypassFrontGPI0. Applies to: CoaXPress |
![]() | BypassFrontGPI1 | The output source is set to BypassFrontGPI1. Applies to: CoaXPress |
![]() | BypassFrontGPI2 | The output source is set to BypassFrontGPI2. Applies to: CoaXPress |
![]() | BypassFrontGPI3 | The output source is set to BypassFrontGPI3. Applies to: CoaXPress |
![]() | CamAPulseGenerator0 | The output source is set to CamAPulseGenerator0. Applies to: CoaXPress |
![]() | CamAPulseGenerator1 | The output source is set to CamAPulseGenerator1. Applies to: CoaXPress |
![]() | CamAPulseGenerator2 | The output source is set to CamAPulseGenerator2. Applies to: CoaXPress |
![]() | CamAPulseGenerator3 | The output source is set to CamAPulseGenerator3. Applies to: CoaXPress |
![]() | GND | The output source is set to GND. Applies to: CoaXPress |
![]() | Name | The full name of TriggerCameraOutSelect (Overrides ParameterListEnum.Name.) |
![]() | NotBypassFronGPI0 | The output source is set to NotBypassFrontGPI0. Applies to: CoaXPress |
![]() | NotBypassFronGPI1 | The output source is set to NotBypassFrontGPI1. Applies to: CoaXPress |
![]() | NotBypassFronGPI2 | The output source is set to NotBypassFrontGPI2. Applies to: CoaXPress |
![]() | NotBypassFronGPI3 | The output source is set to NotBypassFrontGPI3. Applies to: CoaXPress |
![]() | NotCamAPulseGenerator0 | The output source is set to NotCamAPulseGenerator0. Applies to: CoaXPress |
![]() | NotCamAPulseGenerator1 | The output source is set to NotCamAPulseGenerator1. Applies to: CoaXPress |
![]() | NotCamAPulseGenerator2 | The output source is set to NotCamAPulseGenerator2. Applies to: CoaXPress |
![]() | NotCamAPulseGenerator3 | The output source is set to NotCamAPulseGenerator3. Applies to: CoaXPress |
![]() | NotPulseGenerator0 | The output source is set to NotPulseGenerator0. Applies to: CoaXPress |
![]() | NotPulseGenerator1 | The output source is set to NotPulseGenerator1. Applies to: CoaXPress |
![]() | NotPulseGenerator2 | The output source is set to NotPulseGenerator2. Applies to: CoaXPress |
![]() | NotPulseGenerator3 | The output source is set to NotPulseGenerator3. Applies to: CoaXPress |
![]() | PulseGenerator0 | The output source is set to PulseGenerator0. Applies to: CoaXPress |
![]() | PulseGenerator1 | The output source is set to PulseGenerator1. Applies to: CoaXPress |
![]() | PulseGenerator2 | The output source is set to PulseGenerator2. Applies to: CoaXPress |
![]() | PulseGenerator3 | The output source is set to PulseGenerator3. Applies to: CoaXPress |
![]() | VCC | The output source is set to VCC. Applies to: CoaXPress |
Methods#
| Name | Description | |
|---|---|---|
![]() | ToString | The full name of TriggerCameraOutSelect (Overrides Object.ToString()()()().) |
PLTransportLayer.TriggerCameraOutSelectEnum.ToString Method#
The full name of TriggerCameraOutSelect
Return Value#
Type: String
Returns the full name of TriggerCameraOutSelect
PLTransportLayer.TriggerCameraOutSelectEnum Constructor#
Initializes a new instance of the PLTransportLayer.TriggerCameraOutSelectEnum class
PLTransportLayer.TriggerCameraOutSelectEnum.BypassFrontGPI0 Property#
The output source is set to BypassFrontGPI0.
Applies to: CoaXPress
PLTransportLayer.TriggerCameraOutSelectEnum.BypassFrontGPI1 Property#
The output source is set to BypassFrontGPI1.
Applies to: CoaXPress
PLTransportLayer.TriggerCameraOutSelectEnum.BypassFrontGPI2 Property#
The output source is set to BypassFrontGPI2.
Applies to: CoaXPress
PLTransportLayer.TriggerCameraOutSelectEnum.BypassFrontGPI3 Property#
The output source is set to BypassFrontGPI3.
Applies to: CoaXPress
PLTransportLayer.TriggerCameraOutSelectEnum.CamAPulseGenerator0 Property#
The output source is set to CamAPulseGenerator0.
Applies to: CoaXPress
PLTransportLayer.TriggerCameraOutSelectEnum.CamAPulseGenerator1 Property#
The output source is set to CamAPulseGenerator1.
Applies to: CoaXPress
PLTransportLayer.TriggerCameraOutSelectEnum.CamAPulseGenerator2 Property#
The output source is set to CamAPulseGenerator2.
Applies to: CoaXPress
PLTransportLayer.TriggerCameraOutSelectEnum.CamAPulseGenerator3 Property#
The output source is set to CamAPulseGenerator3.
Applies to: CoaXPress
PLTransportLayer.TriggerCameraOutSelectEnum.GND Property#
The output source is set to GND.
Applies to: CoaXPress
PLTransportLayer.TriggerCameraOutSelectEnum.Name Property#
The full name of TriggerCameraOutSelect
PLTransportLayer.TriggerCameraOutSelectEnum.NotBypassFronGPI0 Property#
The output source is set to NotBypassFrontGPI0.
Applies to: CoaXPress
PLTransportLayer.TriggerCameraOutSelectEnum.NotBypassFronGPI1 Property#
The output source is set to NotBypassFrontGPI1.
Applies to: CoaXPress
PLTransportLayer.TriggerCameraOutSelectEnum.NotBypassFronGPI2 Property#
The output source is set to NotBypassFrontGPI2.
Applies to: CoaXPress
PLTransportLayer.TriggerCameraOutSelectEnum.NotBypassFronGPI3 Property#
The output source is set to NotBypassFrontGPI3.
Applies to: CoaXPress
PLTransportLayer.TriggerCameraOutSelectEnum.NotCamAPulseGenerator0 Property#
The output source is set to NotCamAPulseGenerator0.
Applies to: CoaXPress
PLTransportLayer.TriggerCameraOutSelectEnum.NotCamAPulseGenerator1 Property#
The output source is set to NotCamAPulseGenerator1.
Applies to: CoaXPress
PLTransportLayer.TriggerCameraOutSelectEnum.NotCamAPulseGenerator2 Property#
The output source is set to NotCamAPulseGenerator2.
Applies to: CoaXPress
PLTransportLayer.TriggerCameraOutSelectEnum.NotCamAPulseGenerator3 Property#
The output source is set to NotCamAPulseGenerator3.
Applies to: CoaXPress
PLTransportLayer.TriggerCameraOutSelectEnum.NotPulseGenerator0 Property#
The output source is set to NotPulseGenerator0.
Applies to: CoaXPress
PLTransportLayer.TriggerCameraOutSelectEnum.NotPulseGenerator1 Property#
The output source is set to NotPulseGenerator1.
Applies to: CoaXPress
PLTransportLayer.TriggerCameraOutSelectEnum.NotPulseGenerator2 Property#
The output source is set to NotPulseGenerator2.
Applies to: CoaXPress
PLTransportLayer.TriggerCameraOutSelectEnum.NotPulseGenerator3 Property#
The output source is set to NotPulseGenerator3.
Applies to: CoaXPress
PLTransportLayer.TriggerCameraOutSelectEnum.PulseGenerator0 Property#
The output source is set to PulseGenerator0.
Applies to: CoaXPress
PLTransportLayer.TriggerCameraOutSelectEnum.PulseGenerator1 Property#
The output source is set to PulseGenerator1.
Applies to: CoaXPress
PLTransportLayer.TriggerCameraOutSelectEnum.PulseGenerator2 Property#
The output source is set to PulseGenerator2.
Applies to: CoaXPress
PLTransportLayer.TriggerCameraOutSelectEnum.PulseGenerator3 Property#
The output source is set to PulseGenerator3.
Applies to: CoaXPress
PLTransportLayer.TriggerCameraOutSelectEnum.VCC Property#
The output source is set to VCC.
Applies to: CoaXPress