Skip to content
STAGING SERVER

PLTransportLayer.ImageTriggerModeEnum Class#

Sets the trigger mode for the image generation. An image trigger can define the start and length of an image. FreeRun: All incoming lines received from the camera are accepted. Image size is defined by the ROI. ASync_External_Trigger: At the rising edge of an accepted image trigger input signal, a new frame is started and incoming lines are appended to an image up to ROI-Height. A new rising edge of the image trigger is only accepted after the current frame is finished. Gated_External_Trigger: In gated mode, the input signal active state Sets the height of the resulting frame. ROI-Height is the maximum height. _Multibuffer modes can handle a certain number of lines for multiple frames of ROI size.

Applies to: CoaXPress

Visibility: Expert

The feature documentation may provide more information.

Inheritance Hierarchy#

System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLTransportLayer.ImageTriggerModeEnum

Constructors#

 NameDescription
Public methodPLTransportLayer.ImageTriggerModeEnum Initializes a new instance of the PLTransportLayer.ImageTriggerModeEnum class
 

Properties#

 NameDescription
Public propertyAsyncExternalTrigger

Trigger mode is set to Async External Trigger.

Applies to: CoaXPress

Public propertyAsyncExternalTriggerMultiframe

Trigger mode is set to Async External Trigger Multiframe.

Applies to: CoaXPress

Public propertyAsyncGatedTrigger

Trigger mode is set to Async Gated Trigger.

Applies to: CoaXPress

Public propertyAsyncGatedTriggerMultiframe

Trigger mode is set to Async Gated Trigger Multiframe.

Applies to: CoaXPress

Public propertyfreeRun

Free run mode is enabled.

Applies to: CoaXPress

Public propertyName The full name of ImageTriggerMode (Overrides ParameterListEnum.Name.)
 

Methods#

 NameDescription
Public methodToString The full name of ImageTriggerMode (Overrides Object.ToString()()()().)
 

PLTransportLayer.ImageTriggerModeEnum.ToString Method#

The full name of ImageTriggerMode

Return Value#

Type: String
Returns the full name of ImageTriggerMode

PLTransportLayer.ImageTriggerModeEnum Constructor#

Initializes a new instance of the PLTransportLayer.ImageTriggerModeEnum class

PLTransportLayer.ImageTriggerModeEnum.AsyncExternalTrigger Property#

Trigger mode is set to Async External Trigger.

Applies to: CoaXPress

PLTransportLayer.ImageTriggerModeEnum.AsyncExternalTriggerMultiframe Property#

Trigger mode is set to Async External Trigger Multiframe.

Applies to: CoaXPress

PLTransportLayer.ImageTriggerModeEnum.AsyncGatedTrigger Property#

Trigger mode is set to Async Gated Trigger.

Applies to: CoaXPress

PLTransportLayer.ImageTriggerModeEnum.AsyncGatedTriggerMultiframe Property#

Trigger mode is set to Async Gated Trigger Multiframe.

Applies to: CoaXPress

PLTransportLayer.ImageTriggerModeEnum.freeRun Property#

Free run mode is enabled.

Applies to: CoaXPress

PLTransportLayer.ImageTriggerModeEnum.Name Property#

The full name of ImageTriggerMode