PLInterface.DeviceAccessStatusEnum Class#
Applies to: CoaXPress and blaze
Visibility: Expert
Selected by: DeviceSelector
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLInterface.DeviceAccessStatusEnum
Constructors#
| Name | Description | |
|---|---|---|
|  | PLInterface.DeviceAccessStatusEnum | Initializes a new instance of the PLInterface.DeviceAccessStatusEnum class | 
Properties#
| Name | Description | |
|---|---|---|
|  | Busy | The device is already opened by another entity. Applies to: CoaXPress and blaze | 
|  | Name | The full name of DeviceAccessStatus (Overrides ParameterListEnum.Name.) | 
|  | NoAccess | You can't connect to the device. Applies to: CoaXPress and blaze | 
|  | OpenReadOnly | The device is opened in Read-only mode by this GenTL host. Applies to: CoaXPress and blaze | 
|  | OpenReadWrite | The device is opened in Read/Write mode by this GenTL host. Applies to: CoaXPress and blaze | 
|  | ReadOnly | The device offers read-only access. Applies to: CoaXPress and blaze | 
|  | ReadWrite | The device offers read/write access. Applies to: CoaXPress and blaze | 
|  | Unknown | The status is unknown. Applies to: CoaXPress and blaze | 
Methods#
| Name | Description | |
|---|---|---|
|  | ToString | The full name of DeviceAccessStatus (Overrides Object.ToString()()()().) | 
PLInterface.DeviceAccessStatusEnum.ToString Method#
The full name of DeviceAccessStatus
Return Value#
Type: String
Returns the full name of DeviceAccessStatus
PLInterface.DeviceAccessStatusEnum Constructor#
Initializes a new instance of the PLInterface.DeviceAccessStatusEnum class
PLInterface.DeviceAccessStatusEnum.Busy Property#
The device is already opened by another entity.
Applies to: CoaXPress and blaze
PLInterface.DeviceAccessStatusEnum.Name Property#
The full name of DeviceAccessStatus
PLInterface.DeviceAccessStatusEnum.NoAccess Property#
You can't connect to the device.
Applies to: CoaXPress and blaze
PLInterface.DeviceAccessStatusEnum.OpenReadOnly Property#
The device is opened in Read-only mode by this GenTL host.
Applies to: CoaXPress and blaze
PLInterface.DeviceAccessStatusEnum.OpenReadWrite Property#
The device is opened in Read/Write mode by this GenTL host.
Applies to: CoaXPress and blaze
PLInterface.DeviceAccessStatusEnum.ReadOnly Property#
The device offers read-only access.
Applies to: CoaXPress and blaze
PLInterface.DeviceAccessStatusEnum.ReadWrite Property#
The device offers read/write access.
Applies to: CoaXPress and blaze
PLInterface.DeviceAccessStatusEnum.Unknown Property#
The status is unknown.
Applies to: CoaXPress and blaze