PLInterface.CxpLinkConfigurationEnum Class#
Applies to: CoaXPress
Visibility: Beginner
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLInterface.CxpLinkConfigurationEnum
Constructors#
| Name | Description | |
|---|---|---|
|  | PLInterface.CxpLinkConfigurationEnum | Initializes a new instance of the PLInterface.CxpLinkConfigurationEnum class | 
Properties#
| Name | Description | |
|---|---|---|
|  | Auto | Link speed is controlled automatically. Applies to: CoaXPress | 
|  | CXP1_X1 | 1 connection is operating at CXP-1 speed (1.25 Gbps). Applies to: CoaXPress | 
|  | CXP10_X1 | 1 connection is operating at CXP-10 speed (10.0 Gbps). Applies to: CoaXPress | 
|  | CXP12_X1 | 1 connection is operating at CXP-12 speed (12.50 Gbps). Applies to: CoaXPress | 
|  | CXP2_X1 | 1 connection is operating at CXP-2 speed (2.50 Gbps). Applies to: CoaXPress | 
|  | CXP3_X1 | 1 connection is operating at CXP-3 speed (3.125 Gbps). Applies to: CoaXPress | 
|  | CXP5_X1 | 1 connection is operating at CXP-5 speed (5.00 Gbps). Applies to: CoaXPress | 
|  | CXP6_X1 | 1 connection is operating at CXP-6 speed (6.25 Gbps). Applies to: CoaXPress | 
|  | Name | The full name of CxpLinkConfiguration (Overrides ParameterListEnum.Name.) | 
Methods#
| Name | Description | |
|---|---|---|
|  | ToString | The full name of CxpLinkConfiguration (Overrides Object.ToString()()()().) | 
PLInterface.CxpLinkConfigurationEnum.ToString Method#
The full name of CxpLinkConfiguration
Return Value#
Type: String
Returns the full name of CxpLinkConfiguration
PLInterface.CxpLinkConfigurationEnum Constructor#
Initializes a new instance of the PLInterface.CxpLinkConfigurationEnum class
PLInterface.CxpLinkConfigurationEnum.Auto Property#
Link speed is controlled automatically.
Applies to: CoaXPress
PLInterface.CxpLinkConfigurationEnum.CXP10_X1 Property#
1 connection is operating at CXP-10 speed (10.0 Gbps).
Applies to: CoaXPress
PLInterface.CxpLinkConfigurationEnum.CXP12_X1 Property#
1 connection is operating at CXP-12 speed (12.50 Gbps).
Applies to: CoaXPress
PLInterface.CxpLinkConfigurationEnum.CXP1_X1 Property#
1 connection is operating at CXP-1 speed (1.25 Gbps).
Applies to: CoaXPress
PLInterface.CxpLinkConfigurationEnum.CXP2_X1 Property#
1 connection is operating at CXP-2 speed (2.50 Gbps).
Applies to: CoaXPress
PLInterface.CxpLinkConfigurationEnum.CXP3_X1 Property#
1 connection is operating at CXP-3 speed (3.125 Gbps).
Applies to: CoaXPress
PLInterface.CxpLinkConfigurationEnum.CXP5_X1 Property#
1 connection is operating at CXP-5 speed (5.00 Gbps).
Applies to: CoaXPress
PLInterface.CxpLinkConfigurationEnum.CXP6_X1 Property#
1 connection is operating at CXP-6 speed (6.25 Gbps).
Applies to: CoaXPress
PLInterface.CxpLinkConfigurationEnum.Name Property#
The full name of CxpLinkConfiguration