PLCamera.FrequencyConverterInputSourceEnum Class#
Applies to: CameraLink and ace GigE
Visibility: Expert
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.FrequencyConverterInputSourceEnum
Constructors#
| Name | Description | |
|---|---|---|
![]() | PLCamera.FrequencyConverterInputSourceEnum | Initializes a new instance of the PLCamera.FrequencyConverterInputSourceEnum class |
Properties#
| Name | Description | |
|---|---|---|
![]() | CC1 | CC1 is selected as the source signal for the frequency converter module. Applies to: CameraLink and ace GigE |
![]() | CC2 | CC2 is selected as the source signal for the frequency converter module. Applies to: CameraLink and ace GigE |
![]() | CC3 | CC3 is selected as the source signal for the frequency converter module. Applies to: CameraLink and ace GigE |
![]() | CC4 | CC4 is selected as the source signal for the frequency converter module. Applies to: CameraLink and ace GigE |
![]() | Line1 | Line 1 is selected as the input source for the frequency converter module. Applies to: CameraLink and ace GigE |
![]() | Line2 | Line 2 is selected as the input source for the frequency converter module. Applies to: CameraLink and ace GigE |
![]() | Line3 | Line 3 is selected as the input source for the frequency converter module. Applies to: CameraLink and ace GigE |
![]() | Line4 | Line 4 is selected as the input source for the frequency converter module. Applies to: CameraLink and ace GigE |
![]() | Line5 | Selects line 5 as the input source for the frequency converter module. Applies to: CameraLink and ace GigE |
![]() | Line6 | Selects line 6 as the input source for the frequency converter module. Applies to: CameraLink and ace GigE |
![]() | Line7 | Selects line 7 as the input source for the frequency converter module. Applies to: CameraLink and ace GigE |
![]() | Line8 | Selects line 8 as the input source for the frequency converter module. Applies to: CameraLink and ace GigE |
![]() | Name | The full name of FrequencyConverterInputSource (Overrides ParameterListEnum.Name.) |
![]() | ShaftEncoderModuleOut | The output of the shaft encoder module is selected as the input source for the frequency converter module. Applies to: CameraLink and ace GigE |
Methods#
| Name | Description | |
|---|---|---|
![]() | ToString | The full name of FrequencyConverterInputSource (Overrides Object.ToString()()()().) |
PLCamera.FrequencyConverterInputSourceEnum.ToString Method#
The full name of FrequencyConverterInputSource
Return Value#
Type: String
Returns the full name of FrequencyConverterInputSource
PLCamera.FrequencyConverterInputSourceEnum Constructor#
Initializes a new instance of the PLCamera.FrequencyConverterInputSourceEnum class
PLCamera.FrequencyConverterInputSourceEnum.CC1 Property#
CC1 is selected as the source signal for the frequency converter module.
Applies to: CameraLink and ace GigE
PLCamera.FrequencyConverterInputSourceEnum.CC2 Property#
CC2 is selected as the source signal for the frequency converter module.
Applies to: CameraLink and ace GigE
PLCamera.FrequencyConverterInputSourceEnum.CC3 Property#
CC3 is selected as the source signal for the frequency converter module.
Applies to: CameraLink and ace GigE
PLCamera.FrequencyConverterInputSourceEnum.CC4 Property#
CC4 is selected as the source signal for the frequency converter module.
Applies to: CameraLink and ace GigE
PLCamera.FrequencyConverterInputSourceEnum.Line1 Property#
Line 1 is selected as the input source for the frequency converter module.
Applies to: CameraLink and ace GigE
PLCamera.FrequencyConverterInputSourceEnum.Line2 Property#
Line 2 is selected as the input source for the frequency converter module.
Applies to: CameraLink and ace GigE
PLCamera.FrequencyConverterInputSourceEnum.Line3 Property#
Line 3 is selected as the input source for the frequency converter module.
Applies to: CameraLink and ace GigE
PLCamera.FrequencyConverterInputSourceEnum.Line4 Property#
Line 4 is selected as the input source for the frequency converter module.
Applies to: CameraLink and ace GigE
PLCamera.FrequencyConverterInputSourceEnum.Line5 Property#
Selects line 5 as the input source for the frequency converter module.
Applies to: CameraLink and ace GigE
PLCamera.FrequencyConverterInputSourceEnum.Line6 Property#
Selects line 6 as the input source for the frequency converter module.
Applies to: CameraLink and ace GigE
PLCamera.FrequencyConverterInputSourceEnum.Line7 Property#
Selects line 7 as the input source for the frequency converter module.
Applies to: CameraLink and ace GigE
PLCamera.FrequencyConverterInputSourceEnum.Line8 Property#
Selects line 8 as the input source for the frequency converter module.
Applies to: CameraLink and ace GigE
PLCamera.FrequencyConverterInputSourceEnum.Name Property#
The full name of FrequencyConverterInputSource
PLCamera.FrequencyConverterInputSourceEnum.ShaftEncoderModuleOut Property#
The output of the shaft encoder module is selected as the input source for the frequency converter module.
Applies to: CameraLink and ace GigE