PLCamera.ExpertFeatureAccessSelectorEnum Class#
Applies to: CameraLink, ace GigE and ace USB
Visibility: Guru
Selecting Parameters: ExpertFeatureAccessKey, ExpertFeatureEnable
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
  Basler.Pylon.ParameterListEnum
    Basler.Pylon.PLCamera.ExpertFeatureAccessSelectorEnum
Constructors#
| Name | Description | |
|---|---|---|
|  | PLCamera.ExpertFeatureAccessSelectorEnum | Initializes a new instance of the PLCamera.ExpertFeatureAccessSelectorEnum class | 
Properties#
| Name | Description | |
|---|---|---|
|  | ExpertFeature1 | Expert Feature 1 can be configured. Applies to: CameraLink, ace GigE and ace USB | 
|  | ExpertFeature1_Legacy | Expert Feature 1 (Legacy) can be configured. Applies to: CameraLink and ace GigE | 
|  | ExpertFeature10 | Expert Feature 10 can be configured. Applies to: ace GigE and ace USB | 
|  | ExpertFeature11 | Expert Feature 11 can be configured. Applies to: ace GigE and ace USB | 
|  | ExpertFeature2 | Expert Feature 2 can be configured. Applies to: CameraLink, ace GigE and ace USB | 
|  | ExpertFeature3 | Expert Feature 3 can be configured. Applies to: CameraLink, ace GigE and ace USB | 
|  | ExpertFeature4 | Expert Feature 4 can be configured. Applies to: CameraLink, ace GigE and ace USB | 
|  | ExpertFeature5 | Expert Feature 5 can be configured. Applies to: CameraLink, ace GigE and ace USB | 
|  | ExpertFeature6 | Expert Feature 6 can be configured. Applies to: CameraLink, ace GigE and ace USB | 
|  | ExpertFeature7 | Expert Feature 7 can be configured. Applies to: CameraLink, ace GigE and ace USB | 
|  | ExpertFeature8 | Expert Feature 8 can be configured. Applies to: ace GigE and ace USB | 
|  | ExpertFeature9 | Expert Feature 9 can be configured. Applies to: ace GigE and ace USB | 
|  | Name | The full name of ExpertFeatureAccessSelector (Overrides ParameterListEnum.Name.) | 
Methods#
| Name | Description | |
|---|---|---|
|  | ToString | The full name of ExpertFeatureAccessSelector (Overrides Object.ToString()()()().) | 
PLCamera.ExpertFeatureAccessSelectorEnum.ToString Method#
The full name of ExpertFeatureAccessSelector
Return Value#
Type: String
Returns the full name of ExpertFeatureAccessSelector
PLCamera.ExpertFeatureAccessSelectorEnum Constructor#
Initializes a new instance of the PLCamera.ExpertFeatureAccessSelectorEnum class
PLCamera.ExpertFeatureAccessSelectorEnum.ExpertFeature1 Property#
Expert Feature 1 can be configured.
Applies to: CameraLink, ace GigE and ace USB
PLCamera.ExpertFeatureAccessSelectorEnum.ExpertFeature10 Property#
Expert Feature 10 can be configured.
Applies to: ace GigE and ace USB
PLCamera.ExpertFeatureAccessSelectorEnum.ExpertFeature11 Property#
Expert Feature 11 can be configured.
Applies to: ace GigE and ace USB
PLCamera.ExpertFeatureAccessSelectorEnum.ExpertFeature1_Legacy Property#
Expert Feature 1 (Legacy) can be configured.
Applies to: CameraLink and ace GigE
PLCamera.ExpertFeatureAccessSelectorEnum.ExpertFeature2 Property#
Expert Feature 2 can be configured.
Applies to: CameraLink, ace GigE and ace USB
PLCamera.ExpertFeatureAccessSelectorEnum.ExpertFeature3 Property#
Expert Feature 3 can be configured.
Applies to: CameraLink, ace GigE and ace USB
PLCamera.ExpertFeatureAccessSelectorEnum.ExpertFeature4 Property#
Expert Feature 4 can be configured.
Applies to: CameraLink, ace GigE and ace USB
PLCamera.ExpertFeatureAccessSelectorEnum.ExpertFeature5 Property#
Expert Feature 5 can be configured.
Applies to: CameraLink, ace GigE and ace USB
PLCamera.ExpertFeatureAccessSelectorEnum.ExpertFeature6 Property#
Expert Feature 6 can be configured.
Applies to: CameraLink, ace GigE and ace USB
PLCamera.ExpertFeatureAccessSelectorEnum.ExpertFeature7 Property#
Expert Feature 7 can be configured.
Applies to: CameraLink, ace GigE and ace USB
PLCamera.ExpertFeatureAccessSelectorEnum.ExpertFeature8 Property#
Expert Feature 8 can be configured.
Applies to: ace GigE and ace USB
PLCamera.ExpertFeatureAccessSelectorEnum.ExpertFeature9 Property#
Expert Feature 9 can be configured.
Applies to: ace GigE and ace USB
PLCamera.ExpertFeatureAccessSelectorEnum.Name Property#
The full name of ExpertFeatureAccessSelector