PLCamera.CxpLinkConfigurationStatusEnum Class#
Applies to: ace 2 CXP, boost CoaXPress, racer 2 CXP and racer 2S CXP
Visibility: Beginner
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.CxpLinkConfigurationStatusEnum
Constructors#
| Name | Description | |
|---|---|---|
![]() | PLCamera.CxpLinkConfigurationStatusEnum | Initializes a new instance of the PLCamera.CxpLinkConfigurationStatusEnum class |
Properties#
| Name | Description | |
|---|---|---|
![]() | Auto | The link configuration is set to automatic discovery. Applies to: ace 2 CXP, boost CoaXPress, racer 2 CXP and racer 2S CXP |
![]() | CXP10_X1 | The link configuration is set to 1 connection operating at CXP-10 speed (10 Gbps). Applies to: ace 2 CXP, boost CoaXPress, racer 2 CXP and racer 2S CXP |
![]() | CXP10_X2 | The link configuration is set to 2 connections operating at CXP-10 speed (10 Gbps). Applies to: boost CoaXPress and racer 2 CXP |
![]() | CXP12_X1 | The link configuration is set to 1 connection operating at CXP-12 speed (12.5 Gbps). Applies to: ace 2 CXP, boost CoaXPress, racer 2 CXP and racer 2S CXP |
![]() | CXP12_X2 | The link configuration is set to 2 connections operating at CXP-12 speed (12.5 Gbps). Applies to: boost CoaXPress and racer 2 CXP |
![]() | CXP2_X1 | The link configuration is set to 1 connection operating at CXP-2 speed (2.5 Gbps). Applies to: ace 2 CXP, boost CoaXPress, racer 2 CXP and racer 2S CXP |
![]() | CXP2_X2 | The link configuration is set to 2 connections operating at CXP-2 speed (2.5 Gbps). Applies to: boost CoaXPress and racer 2 CXP |
![]() | CXP3_X1 | The link configuration is set to 1 connection operating at CXP-3 speed (3.125 Gbps). Applies to: ace 2 CXP, boost CoaXPress, racer 2 CXP and racer 2S CXP |
![]() | CXP3_X2 | The link configuration is set to 2 connections operating at CXP-3 speed (3.125 Gbps). Applies to: boost CoaXPress and racer 2 CXP |
![]() | CXP5_X1 | The link configuration is set to 1 connection operating at CXP-5 speed (5 Gbps). Applies to: ace 2 CXP, boost CoaXPress, racer 2 CXP and racer 2S CXP |
![]() | CXP5_X2 | The link configuration is set to 2 connections operating at CXP-5 speed (5 Gbps). Applies to: boost CoaXPress and racer 2 CXP |
![]() | CXP6_X1 | The link configuration is set to 1 connection operating at CXP-6 speed (6.25 Gbps). Applies to: ace 2 CXP, boost CoaXPress, racer 2 CXP and racer 2S CXP |
![]() | CXP6_X2 | The link configuration is set to 2 connections operating at CXP-6 speed (6.25 Gbps). Applies to: boost CoaXPress and racer 2 CXP |
![]() | Name | The full name of CxpLinkConfigurationStatus (Overrides ParameterListEnum.Name.) |
Methods#
| Name | Description | |
|---|---|---|
![]() | ToString | The full name of CxpLinkConfigurationStatus (Overrides Object.ToString()()()().) |
PLCamera.CxpLinkConfigurationStatusEnum.ToString Method#
The full name of CxpLinkConfigurationStatus
Return Value#
Type: String
Returns the full name of CxpLinkConfigurationStatus
PLCamera.CxpLinkConfigurationStatusEnum Constructor#
Initializes a new instance of the PLCamera.CxpLinkConfigurationStatusEnum class
PLCamera.CxpLinkConfigurationStatusEnum.Auto Property#
The link configuration is set to automatic discovery.
Applies to: ace 2 CXP, boost CoaXPress, racer 2 CXP and racer 2S CXP
PLCamera.CxpLinkConfigurationStatusEnum.CXP10_X1 Property#
The link configuration is set to 1 connection operating at CXP-10 speed (10 Gbps).
Applies to: ace 2 CXP, boost CoaXPress, racer 2 CXP and racer 2S CXP
PLCamera.CxpLinkConfigurationStatusEnum.CXP10_X2 Property#
The link configuration is set to 2 connections operating at CXP-10 speed (10 Gbps).
Applies to: boost CoaXPress and racer 2 CXP
PLCamera.CxpLinkConfigurationStatusEnum.CXP12_X1 Property#
The link configuration is set to 1 connection operating at CXP-12 speed (12.5 Gbps).
Applies to: ace 2 CXP, boost CoaXPress, racer 2 CXP and racer 2S CXP
PLCamera.CxpLinkConfigurationStatusEnum.CXP12_X2 Property#
The link configuration is set to 2 connections operating at CXP-12 speed (12.5 Gbps).
Applies to: boost CoaXPress and racer 2 CXP
PLCamera.CxpLinkConfigurationStatusEnum.CXP2_X1 Property#
The link configuration is set to 1 connection operating at CXP-2 speed (2.5 Gbps).
Applies to: ace 2 CXP, boost CoaXPress, racer 2 CXP and racer 2S CXP
PLCamera.CxpLinkConfigurationStatusEnum.CXP2_X2 Property#
The link configuration is set to 2 connections operating at CXP-2 speed (2.5 Gbps).
Applies to: boost CoaXPress and racer 2 CXP
PLCamera.CxpLinkConfigurationStatusEnum.CXP3_X1 Property#
The link configuration is set to 1 connection operating at CXP-3 speed (3.125 Gbps).
Applies to: ace 2 CXP, boost CoaXPress, racer 2 CXP and racer 2S CXP
PLCamera.CxpLinkConfigurationStatusEnum.CXP3_X2 Property#
The link configuration is set to 2 connections operating at CXP-3 speed (3.125 Gbps).
Applies to: boost CoaXPress and racer 2 CXP
PLCamera.CxpLinkConfigurationStatusEnum.CXP5_X1 Property#
The link configuration is set to 1 connection operating at CXP-5 speed (5 Gbps).
Applies to: ace 2 CXP, boost CoaXPress, racer 2 CXP and racer 2S CXP
PLCamera.CxpLinkConfigurationStatusEnum.CXP5_X2 Property#
The link configuration is set to 2 connections operating at CXP-5 speed (5 Gbps).
Applies to: boost CoaXPress and racer 2 CXP
PLCamera.CxpLinkConfigurationStatusEnum.CXP6_X1 Property#
The link configuration is set to 1 connection operating at CXP-6 speed (6.25 Gbps).
Applies to: ace 2 CXP, boost CoaXPress, racer 2 CXP and racer 2S CXP
PLCamera.CxpLinkConfigurationStatusEnum.CXP6_X2 Property#
The link configuration is set to 2 connections operating at CXP-6 speed (6.25 Gbps).
Applies to: boost CoaXPress and racer 2 CXP
PLCamera.CxpLinkConfigurationStatusEnum.Name Property#
The full name of CxpLinkConfigurationStatus