PLCamera.BLCSerialReceiveQueueStatusEnum Class#
Applies to: ace GigE and ace USB
Visibility: Guru
The feature documentation may provide more information.
Inheritance Hierarchy#
System.Object
Basler.Pylon.ParameterListEnum
Basler.Pylon.PLCamera.BLCSerialReceiveQueueStatusEnum
Constructors#
Name | Description | |
---|---|---|
![]() | PLCamera.BLCSerialReceiveQueueStatusEnum | Initializes a new instance of the PLCamera.BLCSerialReceiveQueueStatusEnum class |
Properties#
Name | Description | |
---|---|---|
![]() | Empty | The receive queue is empty. Applies to: ace GigE and ace USB |
![]() | Filled | The receive queue contains at least one value. Applies to: ace GigE and ace USB |
![]() | Full | The receive queue is full. Applies to: ace GigE and ace USB |
![]() | Name | The full name of BLCSerialReceiveQueueStatus (Overrides ParameterListEnum.Name.) |
Methods#
Name | Description | |
---|---|---|
![]() | ToString | The full name of BLCSerialReceiveQueueStatus (Overrides Object.ToString()()()().) |
PLCamera.BLCSerialReceiveQueueStatusEnum.ToString Method#
The full name of BLCSerialReceiveQueueStatus
Return Value#
Type: String
Returns the full name of BLCSerialReceiveQueueStatus
PLCamera.BLCSerialReceiveQueueStatusEnum Constructor#
Initializes a new instance of the PLCamera.BLCSerialReceiveQueueStatusEnum class
PLCamera.BLCSerialReceiveQueueStatusEnum.Empty Property#
The receive queue is empty.
Applies to: ace GigE and ace USB
PLCamera.BLCSerialReceiveQueueStatusEnum.Filled Property#
The receive queue contains at least one value.
Applies to: ace GigE and ace USB
PLCamera.BLCSerialReceiveQueueStatusEnum.Full Property#
The receive queue is full.
Applies to: ace GigE and ace USB
PLCamera.BLCSerialReceiveQueueStatusEnum.Name Property#
The full name of BLCSerialReceiveQueueStatus