CameraFinder Class#
Inheritance Hierarchy#
System.Object
Basler.Pylon.CameraFinder
Syntax#
C#
VB
The CameraFinder type exposes the following members.
Methods#
| Name | Description | |
|---|---|---|
![]() ![]() | Enumerate() | Retrieves information about cameras connected to the system. |
![]() ![]() | Enumerate(String) | Retrieves information about cameras of a specific type connected to the system. |
![]() ![]() | GetDeviceAccessibilityInfo | Returns information about the accessibility of a camera device. |
CameraFinder.Enumerate Method#
Retrieves information about cameras connected to the system.
Syntax#
C#
VB
Return Value#
Type: List(ICameraInfo)
Returns a list of ICameraInfo objects, one for each camera found. The list is ordered by device type and serial number. Device type order: USB, GigE, Camera Link, other device types ordered by using the < operator, Camera Emulation
Remarks#
The function queries for camera devices connected to the system and returns a list of ICameraInfo objects describing the cameras. The returned information can be used to create a specific Camera object.
Thread Safety: This method is thread-safe.
Error Safety: Can throw exceptions.
CameraFinder.Enumerate Method (String)#
Retrieves information about cameras of a specific type connected to the system.
Syntax#
C#
VB
Parameters#
- deviceType
- Type: System.String
The name of the device type to enumerate connected devices. The static class DeviceType can be used to get a list of valid device class names.
Return Value#
Type: List(ICameraInfo)
Returns a list of ICameraInfo objects, one per camera found. The list is ordered by serial number
Remarks#
The function queries for camera devices of a specific device class connected to the system and returns a list of ICameraInfo objects describing the cameras. The returned information can be used to create a specific Camera object. The static class DeviceType can be used to get a list of valid device type names.
Thread Safety: This method is thread-safe.
Error Safety: Can throw exceptions.
CameraFinder.GetDeviceAccessibilityInfo Method#
Returns information about the accessibility of a camera device.
Syntax#
C#
VB
Public Shared Function GetDeviceAccessibilityInfo (
cameraInfo As ICameraInfo
) As DeviceAccessibilityInfo
Parameters#
- cameraInfo
- Type: Basler.Pylon.ICameraInfo
An ICameraInfo object specifying the camera device of which the state is returned. The Enumerate() methods can be used to retrieve ICameraInfo objects.
Return Value#
Type: DeviceAccessibilityInfo
Returns a DeviceAccessibilityInfo value for the camera device.
Remarks#
This function can be used to check if a camera device is currently reachable. This can be used to prevent errors when opening a camera.
Note |
|---|
Some cameras do not support this feature and may return DeviceAccessibilityInfo.Unknown. |
Error Safety: Can throw exceptions.
CameraFinder.Enumerate Method#
Overload List#
| Name | Description | |
|---|---|---|
![]() ![]() | Enumerate() | Retrieves information about cameras connected to the system. |
![]() ![]() | Enumerate(String) | Retrieves information about cameras of a specific type connected to the system. |


Note