Basler_ImageFormatConverterParams#
Classes#
| Name | |
|---|---|
| class | Basler_ImageFormatConverterParams::CImageFormatConverterParams_Params A parameter class containing all parameters as members that are available for Image Format Converter. |
| class | Basler_ImageFormatConverterParams::CImageFormatConverterParams_Params_v12_0_0 A parameter class containing all parameters as members that are available for Image Format Converter. |
Types#
| Name | |
|---|---|
| enum | InconvertibleEdgeHandlingEnums { InconvertibleEdgeHandling_Clip, InconvertibleEdgeHandling_Extend, InconvertibleEdgeHandling_SetZero} Valid values for InconvertibleEdgeHandling. |
| enum | MonoConversionMethodEnums { MonoConversionMethod_Gamma, MonoConversionMethod_Truncate} Valid values for MonoConversionMethod. |
| enum | OutputBitAlignmentEnums { OutputBitAlignment_LsbAligned, OutputBitAlignment_MsbAligned} Valid values for OutputBitAlignment. |
| enum | OutputOrientationEnums { OutputOrientation_BottomUp, OutputOrientation_TopDown, OutputOrientation_Unchanged} Valid values for OutputOrientation. |
Types Documentation#
enum InconvertibleEdgeHandlingEnums#
| Enumerator | Value | Description |
|---|---|---|
| InconvertibleEdgeHandling_Clip | Rows and columns that can't be converted are removed from the output image - Applies to: ImageFormatConverter. | |
| InconvertibleEdgeHandling_Extend | Rows and columns that can't be converted are filled by extrapolating image data from neighboring rows and columns - Applies to: ImageFormatConverter. | |
| InconvertibleEdgeHandling_SetZero | Rows and columns that can't be converted are set to zero - Applies to: ImageFormatConverter. |
enum MonoConversionMethodEnums#
| Enumerator | Value | Description |
|---|---|---|
| MonoConversionMethod_Gamma | When converting images, Gamma conversion is used - Applies to: ImageFormatConverter. | |
| MonoConversionMethod_Truncate | When converting images, image data is shifted - Applies to: ImageFormatConverter. |
Valid values for MonoConversionMethod.
enum OutputBitAlignmentEnums#
| Enumerator | Value | Description |
|---|---|---|
| OutputBitAlignment_LsbAligned | Image data is aligned with the least significant bit - Applies to: ImageFormatConverter. | |
| OutputBitAlignment_MsbAligned | The data is aligned at the most significant bit - Applies to: ImageFormatConverter. |
Valid values for OutputBitAlignment.
enum OutputOrientationEnums#
| Enumerator | Value | Description |
|---|---|---|
| OutputOrientation_BottomUp | The last row of the image is located at the start of the image buffer - Applies to: ImageFormatConverter. | |
| OutputOrientation_TopDown | The first row of the image is located at the start of the image buffer - Applies to: ImageFormatConverter. | |
| OutputOrientation_Unchanged | The orientation of the image remains the same - Applies to: ImageFormatConverter. |
Valid values for OutputOrientation.