Modules
- GenICam
The GenICam GenApi is used for parameter access in pylon. - Image Handling Support
Besides the Instant Camera classes used for grabbing images pylon offers additional classes that support handling the grabbed images. - Instant Camera
Instant Camera classes make it possible to grab images with a few lines of code reducing the programming effort to a minimum. - Low Level API
Please use the Instant Camera classes whenever possible instead of the Low Level API. - Transport Layer
The Transport Layer Factory or a Transport Layer object are used to enumerate and create pylon Devices.
Updated on 23 September 2022 at 03:12:53