Image Cropper vTool#
By making an image smaller, you also reduce the size of the image that subsequent vTools work with. This may reduce processing time and may help to avoid incorrect results because irrelevant information is removed. You can specify the size of the resulting image manually. Alternatively, you can use the rectangle output from any vTool that outputs rectangles, e.g., the Rectangle Measurements Pro vTool, as input for the CropArea pin to define the resulting image.
情報
The Image Cropper changes the actual image size and therefore also changes the image's coordinate system. This means that you can't return to the original image. If you want to preserve the original image for later use, consider using the ROI Creator vTool. Using the ROI Creator, you can perform operations on just a portion of the original image without losing the original.
Download the pylon Software Suite to use the Image Cropper vTool.

入力#
画像#
Camera vToolから、またはImage Format ConvertervToolなどの画像を出力するvToolから、直接画像を受け入れます。
- データ型:Image
- Image format: 8-bit and 16-bit mono or color images (see Supported Pixel Formats)
CropArea#
Accepts the rectangle output from other vTools to define the resulting image size.
- データタイプ:RectangleF
出力#
画像#
Returns the cropped image with the same data type as the input image.
- データ型:Image
- 画像形式:カラーまたはモノクロ画像(「サポートされるピクセルフォーマット」を参照)
サポートされているPixel Format#
The following pixel formats are supported natively:
- Mono 8
- Mono 16
- Bayer XX 8
- Bayer XX 16
- RGB 8
- BGR 8