Circuit Diagrams (Basler dart M GigE Interface Boards)#
Opto-Coupled Input Line#
The following diagram shows a typical circuit using the opto-coupled input line (Line 1) of a Basler dart M GigE Interface Board. As an example, a TTL or CMOS logic gate is used in the external circuit.
GPIO入力ライン#
The following diagram shows a typical circuit when a GPIO line is set to operate as an input. As an example, Line 3 is connected, and a TTL or CMOS logic gate is used in the external circuit.
次の図は、GPIOラインを使用した外部回路の別の例を示しています。
The following diagram shows the same setup without using an external pull-up resistor:
GPO / GPIO as Output Line#
The following diagram shows a typical circuit when a GPIO line is set to operate as an output. As an example, Line 3 is connected. This circuit only works with devices that accept NPN communication.
The following diagram shows the same setup without using an external pull-up resistor: