Trigger Source#
トリガーソースとして、入力行やソフトウェアコマンドなどを選択できます。
機能を使用する#
トリガーのトリガー方法を設定するには、次の手順を実行します。
TriggerSelector
パラメーターを目的のトリガータイプ(FrameStart
など)に設定します。- パラメーターを
TriggerSource
次のいずれかの値(使用している場合)に設定します:Line1
、Line2
、Line3
、Line4
:選択したトリガーは、I/Oライン1、2、3、または4に電気信号を適用することによってトリガーできます。
I/OラインがGPIOラインの場合は、ラインを入力用に設定する必要があります。ソフトウェア
:選択したトリガーは、TriggerSoftware
コマンドを実行することで起動できます。SoftwareSignal1
、SoftwareSignal2
、SoftwareSignal3
:選択したトリガーは、Software Signal Pulse機能を使用して起動できます。Action1
:選択したトリガーは、Action Commands機能を使用して起動できます。Counter1Active
、Counter2Active
:選択したトリガーは、Counter機能を使用して起動できます。指定されたカウンターがカウントされている間はトリガー信号は高(1)になり、カウントされていない間は低(0)になります。Counter1Start
、Counter2Start
:選択したトリガーは、Counter機能を使用して起動できます。トリガー信号は、指定されたカウンターがカウントを開始するたびに送信されます。Counter1End
、Counter2End
:選択したトリガーは、Counter機能を使用して起動できます。指定されたカウンターがカウントを停止すると、トリガー信号が送信されます。Timer1Active
、Timer2Active
:選択したトリガーは、Timer機能を使用して起動できます。指定されたタイマーが実行されている間はトリガー信号は高(1)になり、実行されていない間は低(0)になります。Timer1End
、Timer2End
:選択したトリガーは、Timer機能を使用して起動できます。トリガー信号は、指定されたタイマー時間が経過するたびに送信されます。PeriodicSignal1
:選択したトリガーは、Periodic Signal機能を使用して起動できます。トリガー信号は繰り返し送信されます。その期間は、BslPeriodicSignalPeriod
パラメーターで定義されます。-
CXPTrigger0
、CXPTrigger1
:選択したトリガーは、CXP-12インターフェイスカードからトリガー信号を受信することによって起動されます。You can find information about configuring the interface card in the Configuring a CXP-12 Interface Card topic. Triggering the camera via the interface card has the following advantages:
- 短いトリガー遅延。
CXP-10またはCXP-12を使用している場合、トリガー精度は0.5µs未満です。CXP-6、CXP-5、またはCXP-3を使用している場合は、トリガー精度は1µs未満です。 - 生成されたI/Oトリガーパケットは、CoaXPressデータケーブルを介してカメラに送信されます。これは、ケーブルのセットアップに役立つ場合があります。
The
CXPTrigger0
andCXPTrigger1
triggers correspond to theLinkTrigger0
andLinkTrigger1
trigger packet definitions in the CoaXPress Standard version 2.0. In version 1.x,LinkTrigger0
is called "rising edge" andLinkTrigger1
is called "falling edge". - 短いトリガー遅延。
特性#
カメラモデル | 使用可能なHardware Trigger Source | 使用可能なSoftware Trigger Source |
---|---|---|
a2A1920-51gcBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A1920-51gcPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A1920-51gmBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A1920-51gmPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A1920-160ucBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A1920-160ucPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A1920-160umBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A1920-160umPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2448-23gcBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2448-23gcPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2448-23gmBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2448-23gmPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2448-75ucBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2448-75ucPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2448-75umBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2448-75umPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2448-105g5cBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2448-105g5mBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2590-22gcBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2590-22gcPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2590-22gmBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2590-22gmPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2590-60ucBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2590-60ucPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2590-60umBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2590-60umPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2600-20gcBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2600-20gcPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2600-20gmBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2600-20gmPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2600-64ucBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2600-64ucPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2600-64umBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2600-64umPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2840-14gcBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2840-14gcPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2840-14gmBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2840-14gmPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2840-48ucBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2840-48ucPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2840-48umBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2840-48umPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2840-67g5cBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A2840-67g5mBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A3840-13gcBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A3840-13gcPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A3840-13gmBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A3840-13gmPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A3840-45ucBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A3840-45ucPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A3840-45umBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A3840-45umPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4096-9gcBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4096-9gcPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4096-9gmBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4096-9gmPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4096-30ucBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4096-30ucPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4096-30umBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4096-30umPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4096-44g5cBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4096-44g5mBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4200-12gcBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4200-12gcPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4200-12gmBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4200-12gmPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4200-40ucBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4200-40ucPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4200-40umBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4200-40umPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4504-5gcBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4504-5gcPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4504-5gmBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4504-5gmPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4504-18ucBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4504-18ucPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4504-18umBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4504-18umPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4504-27g5cBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A4504-27g5mBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5320-7gcBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5320-7gcPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5320-7gmBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5320-7gmPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5320-23ucBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5320-23ucPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5320-23umBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5320-23umPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5320-34g5cBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5320-34g5mBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5328-4gcBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5328-4gcPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5328-4gmBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5328-4gmPRO | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5328-15ucBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5328-15ucPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5328-15umBAS | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5328-15umPRO | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5328-22g5cBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
a2A5328-22g5mBAS | Line 1 Line 2 Line 3 | Action 1 Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Periodic Signal 1 Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
acA640-90gc | ライン1 | Software Action 1 |
acA640-90uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA640-121gm | Line 1 Line 3 | Software Action 1 |
acA640-300gc | Line 1 Line 3 | Software Action 1 |
acA640-300gm | Line 1 Line 3 | Software Action 1 |
acA640-750uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA640-750um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA720-290gc | Line 1 Line 3 | Software Action 1 |
acA720-290gm | Line 1 Line 3 | Software Action 1 |
acA720-520uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA720-520um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA800-200gc | Line 1 Line 3 | Software Action 1 |
acA800-200gm | Line 1 Line 3 | Software Action 1 |
acA800-510uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA800-510um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA1280-60gc | Line1 | ソフトウェア |
acA1280-60gm | ライン1 | ソフトウェア |
acA1300-60gc | ライン1 | Software Action 1 |
acA1300-60gm | ライン1 | Software Action 1 |
acA1300-60gmNIR | ライン1 | Software Action 1 |
acA1300-75gc | Line 1 Line 3 | Software Action 1 |
acA1300-75gm | Line 1 Line 3 | Software Action 1 |
acA1300-200uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA1300-200um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA1440-73gc | Line 1 Line 3 | Software Action 1 |
acA1440-73gm | Line 1 Line 3 | Software Action 1 |
acA1440-220uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA1440-220um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA1600-20gc | ライン1 | Software Action 1 |
acA1600-20uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA1600-60gc | ライン1 | Software Action 1 |
acA1600-60gm | ライン1 | Software Action 1 |
acA1920-25gc | ライン1 | Software Action 1 |
acA1920-25gm | ライン1 | Software Action 1 |
acA1920-25uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA1920-25um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA1920-40gc | Line 1 Line 3 | Software Action 1 |
acA1920-40gm | Line 1 Line 3 | Software Action 1 |
acA1920-40uc | Line 1 Line 2 Line 3 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA1920-40ucMED | Line 1 Line 2 Line 3 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA1920-40um | Line 1 Line 2 Line 3 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA1920-40umMED | Line 1 Line 2 Line 3 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA1920-48gc | Line 1 Line 3 | Software Action 1 |
acA1920-48gm | Line 1 Line 3 | Software Action 1 |
acA1920-50gc | Line 1 Line 3 | Software Action 1 |
acA1920-50gm | Line 1 Line 3 | Software Action 1 |
acA1920-150uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA1920-150um | Line 1 Line 2 Line 3 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA1920-155uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA1920-155ucMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA1920-155um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA1920-155umMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA2000-50gc | ライン1 | Software Action 1 |
acA2000-50gm | ライン1 | Software Action 1 |
acA2000-50gmNIR | ライン1 | Software Action 1 |
acA2000-165uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA2000-165um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA2000-165umNIR | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA2040-25gc | ライン1 | Software Action 1 |
acA2040-25gm | ライン1 | Software Action 1 |
acA2040-25gmNIR | ライン1 | Software Action 1 |
acA2040-35gc | Line 1 Line 3 | Software Action 1 |
acA2040-35gm | Line 1 Line 3 | Software Action 1 |
acA2040-55uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA2040-55um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA2040-90uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA2040-90um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA2040-90umNIR | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA2040-120uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA2040-120um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA2440-20gc | Line 1 Line 3 | Software Action 1 |
acA2440-20gm | Line 1 Line 3 | Software Action 1 |
acA2440-35uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA2440-35ucMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA2440-35um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA2440-35umMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA2440-75uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA2440-75ucMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA2440-75um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA2440-75umMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA2500-14gc | ライン1 | Software Action 1 |
acA2500-14gm | ライン1 | Software Action 1 |
acA2500-14uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA2500-14um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA2500-20gc | Line 1 Line 3 | Software Action 1 |
acA2500-20gcMED | Line 1 Line 3 | Software Action 1 |
acA2500-20gm | Line 1 Line 3 | Software Action 1 |
acA2500-20gmMED | Line 1 Line 3 | Software Action 1 |
acA2500-60uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA2500-60um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA3088-16gc | Line 1 Line 3 | Software Action 1 |
acA3088-16gm | Line 1 Line 3 | Software Action 1 |
acA3088-57uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA3088-57ucMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA3088-57um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA3088-57umMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA3800-10gc | Line 1 Line 3 | Software Action 1 |
acA3800-10gm | Line 1 Line 3 | Software Action 1 |
acA3800-14uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA3800-14um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA4024-8gc | Line 1 Line 3 | Software Action 1 |
acA4024-8gm | Line 1 Line 3 | Software Action 1 |
acA4024-29uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA4024-29um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA4096-11gc | Line 1 Line 3 | Software Action 1 |
acA4096-11gm | Line 1 Line 3 | Software Action 1 |
acA4096-30uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA4096-30ucMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA4096-30um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA4096-30umMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA4096-40uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA4096-40ucMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA4096-40um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA4096-40umMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA4112-8gc | Line 1 Line 3 | Software Action 1 |
acA4112-8gm | Line 1 Line 3 | Software Action 1 |
acA4112-20uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA4112-20ucMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA4112-20um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA4112-20umMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA4112-30uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA4112-30ucMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA4112-30um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA4112-30umMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA4600-7gc | ライン1 | Software Action 1 |
acA4600-10uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA5472-5gc | Line 1 Line 3 | Software Action 1 |
acA5472-5gm | Line 1 Line 3 | Software Action 1 |
acA5472-17uc | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA5472-17ucMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA5472-17um | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
acA5472-17umMED | Line 1 Line 3 Line 4 | Software Software Signal 1 Software Signal 2 Software Signal 3(一部のカメラモデル) |
boA1936-400cc | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA1936-400cm | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA2448-250cc | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA2448-250cm | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA2832-190cc | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA2832-190cm | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA4096-93cc | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA4096-93cm | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA4096-180cc | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA4096-180cm | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA4112-68cc | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA4112-68cm | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA4500-45cc | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA4500-45cm | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA4504-100cc | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA4504-100cm | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA5320-150cc | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA5320-150cm | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA5328-100cc | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA5328-100cm | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA6500-36cc | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA6500-36cm | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA8100-16cc | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
boA8100-16cm | Line 1 Line 2 Line 3 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 CXP Trigger 0 CXP Trigger 1 |
daA720-520uc | Line 1 Line 2 Line 3 Line 4 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
daA720-520um | Line 1 Line 2 Line 3 Line 4 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
daA1280-54uc | Line 1 Line 2 | ソフトウェア |
daA1280-54um | Line 1 Line 2 | ソフトウェア |
daA1440-220uc | Line 1 Line 2 Line 3 Line 4 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
daA1440-220um | Line 1 Line 2 Line 3 Line 4 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
daA1600-60uc | Line 1 Line 2 | ソフトウェア |
daA1600-60um | Line 1 Line 2 | ソフトウェア |
daA1920-15um | Line 1 Line 2 | ソフトウェア |
daA1920-30uc | Line 1 Line 2 | ソフトウェア |
daA1920-30um | Line 1 Line 2 | ソフトウェア |
daA1920-160uc | Line 1 Line 2 Line 3 Line 4 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
daA1920-160um | Line 1 Line 2 Line 3 Line 4 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
daA2448-70uc | Line 1 Line 2 Line 3 Line 4 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
daA2448-70um | Line 1 Line 2 Line 3 Line 4 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
daA2500-14uc | Line 1 Line 2 | ソフトウェア |
daA2500-14um | Line 1 Line 2 | ソフトウェア |
daA3840-45uc | Line 1 Line 2 Line 3 Line 4 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
daA3840-45um | Line 1 Line 2 Line 3 Line 4 | Counter 1 Active Counter 1 End Counter 1 Start Counter 2 Active Counter 2 End Counter 2 Start Timer 1 Active Timer 1 End Timer 2 Active Timer 2 End Software Software Signal 1 Software Signal 2 Software Signal 3 |
puA1280-54uc | None | ソフトウェア |
puA1280-54um | None | ソフトウェア |
puA1600-60uc | None | ソフトウェア |
puA1600-60um | None | ソフトウェア |
puA1920-30uc | None | ソフトウェア |
puA1920-30um | None | ソフトウェア |
puA2500-14uc | None | ソフトウェア |
puA2500-14um | None | ソフトウェア |
サンプルコード#
// Select the Frame Start trigger
camera.TriggerSelector.SetValue(TriggerSelector_FrameStart);
// Set the trigger source to Line 1
camera.TriggerSource.SetValue(TriggerSource_Line1);
INodeMap& nodemap = camera.GetNodeMap();
// Select the Frame Start trigger
CEnumParameter(nodemap, "TriggerSelector").SetValue("FrameStart");
// Set the trigger source to Line 1
CEnumParameter(nodemap, "TriggerSource").SetValue("Line1");
// Select the Frame Start trigger
camera.Parameters[PLCamera.TriggerSelector].SetValue(PLCamera.TriggerSelector.FrameStart);
// Set the trigger source to Line 1
camera.Parameters[PLCamera.TriggerSource].SetValue(PLCamera.TriggerSource.Line1);
/* Macro to check for errors */
#define CHECK(errc) if (GENAPI_E_OK != errc) printErrorAndExit(errc)
GENAPIC_RESULT errRes = GENAPI_E_OK; /* Return value of pylon methods */
/* Select the Frame Start trigger */
errRes = PylonDeviceFeatureFromString(hdev, "TriggerSelector", "FrameStart");
CHECK(errRes);
/* Set the trigger source to Line 1 */
errRes = PylonDeviceFeatureFromString(hdev, "TriggerSource", "Line1");
CHECK(errRes);
pylon Viewerを使用して、パラメーターを簡単に設定することもできます。