3D camera modules

The rc_visard’s 3D camera software consists of the following modules:

  • カメラ (rc_camera)
    acquires image pairs and performs planar rectification for using the camera as a measurement device. Images are provided both for further internal processing by other modules and for external use as GenICam image streams.
  • Stereo matching (rc_stereomatching)
    uses the rectified stereo image pairs to compute 3D depth information such as disparity, error, and confidence images. These are provided as GenICam streams, too.

The Camera and the Stereo matching modules, which acquire image pairs and compute 3D depth information such as disparity, error, and confidence images, are also accessible via the rc_visard’s GigE Vision/GenICam interface.