Skip to content

Software#

You can operate the frame grabber using the Framegrabber SDK or the pylon Camera Software Suite.

However, marathon frame grabbers can't be operated with pylon, and Interface Cards can't be operated with the Framegrabber SDK. Therefore, see in the matrix below which frame grabber can be operated with which software:

Frame Grabber Only Basler Cameras Basler and/or Other Cameras
imaWorx CXP-12 Quad pylon Camera Software Suite Framegrabber SDK
marathon CXP-6/Camera Link Framegrabber SDK Framegrabber SDK
CXP-12 Interface Card 1C/2C/4C pylon Camera Software Suite Framegrabber SDK