Skip to content
STAGING SERVER

Which Basler GigE Cameras Support the Extended ID Mode#

The Extended ID mode is an option that can be activated on Basler GigE cameras to label each acquired image with a block ID up to 64 bit instead of 16 bit. It is defined in the GigE Vision standard and must be enabled on the GigE Vision driver side.

The following Basler GigE cameras support the Extended ID mode:

  • ace U
  • ace L
  • ace 2
  • blaze (since firmware version 4.6.2)
  • racer (since firmware version 2.1.0)

Back to Knowledge Articles